Serial Memory Quick Start Guide

Overview

The NXP Serial Memory Tool is a Visual Studio Code extension that streamlines serial memory configuration and validation for NXP microcontrollers. With an intuitive graphical interface, developers can easily configure memory parameters, validate settings on real hardware, and generate FCB binaries—all without leaving VS Code.

Note: This user guide applies to NXP Serial Memory Tool version 25.12. For the latest updates and information, check the extension marketplace page.

Note: The software is subject to the NXP software license agreement.

Key features

  • Serial memory configuration and validation

  • Real-time validation

  • Integration with Visual Studio Code

  • Support for the RT1180 microcontroller family

  • Import/save capability

  • FCB generation

  • User-friendly UI for creating and modifying the memory lookup table

  • Link a C project to apply configurations changes

System requirements

Supported operating systems

  • Windows 10 (64-bit)

  • Windows 11 (64-bit)

Software requirements

  • Visual Studio Code (the latest version is recommended)

  • Python environment (the tool configures this automatically)

Hardware support

  • RT1180 microcontroller family

Installation

Installing the extension

  • Open Visual Studio Code

  • Go to the Extensions view (Ctrl+Shift+X)

  • Search for “Serial Memory Tool for VS Code”

  • Click Install

Setting up the Python environment

  1. After installation, the Install Toolchain button appears in the tool interface.

    Install Toolchain

  2. To automatically set up the preconfigured Python environment, click the button.

  3. Wait for the installation to complete (this process may take several minutes).

    Install Toolchain Notification

Getting started

Working with Serial Memory Tool

  1. Open VS Code

  2. Access the Serial Memory Tool:

    • Open the Command Palette (Ctrl+Shift+P)

    • Type “NXP Serial Memory Tool” and select

    • Look for the NXP tool icon in the Activity Bar

    Toolbar Icon

  3. Select the target device:

  • Select a processor from the supported devices list.

  • Once a processor is selected, a default Memory Chip is automatically assigned. This chip comes with a standard configuration validated on the EVK board.

    MCU and Memory

  • If the Memory Chip is changed, the memory type is updated automatically in the Configuration page to match the new selection.

    Memory Chip Type

  1. Use the default standard configuration or create a custom configuration:

  • EVK configuration is set by default for the selected device.

  • If needed, adjust the configuration of Memory, FlexSPI Connection, Memory LUT.

  • Memory Information Configuration

    Memory Information Config

  • FlexSPI Connection Configuration

    FlexSPI Connection Config

  • Memory LUT Configuration provides the option to add or remove LUT commands as it is needed for advanced memory configurations.

    Memory LUT Config

  • To save any configuration changes, press Ctrl+S or navigate to File->Save.

    Save configuration

  1. Link an SDK C project (optional):

  • Click the Link C Project button to associate the current configuration with an SDK C project.

    Link C project

  • Select the project folder containing the SDK C project files.

  • Once linked, Editing mode is enabled for configuration modifications. All modified files will be listed in the Modified Files section.

    Editing SDK files

  • Changes are highlighted in the project explorer and can be reviewed before validation.

    Highlighted changes

  1. Board detection:

  • Before connecting, ensure the board is configured to boot in Serial Downloader mode.

  • Connect one cable to the USB_OTG1 for the Serial Downloader interface and the second cable to the Debug USB port for UART communication.

  • A connected board can be detected using the “Refresh current connection” button available in the Connection group.

    Refresh Connection

  • Choose the appropriate COM port in case multiple boards are connected.

  • The connection icon changes and indicates a ‘Connected’ status once the board is detected.

    Board Detection

  1. Validate configuration by executing tests on the target:

Configure test parameters:

  • Click Test, the Test Configuration tab opens to the right.

  • To modify test settings, change test parameters.

  • Upon test parameters changing, validation errors can be displayed in case the selected parameters are not correct.

    Test Configuration

Execute test:

  • Tests cannot be executed unless a board is detected (the Run Test button is disabled).

  • Once a board is detected, the tests Run button gets enabled (green icon).

  • Click the Start button to start the test execution.

  • The pass / Fail status icon is displayed in the left side of the tests tree after the test finishes executing.

    Test Execution

  • The Test execution log is displayed in the Serial Memory Tool for VS Code console that is automatically opened in the bottom once a test is started.

  1. Import configuration:

  • The Import button is located in the top-right corner in the “MCU & Memory” panel.

  • Imported -> A saved configuration can be imported using the import button.

    Import configuration

  1. Generate FCB:

  • The FCB button is available in the top-right corner in the “MCU & Memory” panel.

  • To generate and save FCB binary, use the Generate FCB button.

    Generate FCB

Basic workflow

Start Tool → Select MCU and Memory Chip → Configure Memory Settings → Board detection → Validate Configuration by executing tests on target -> Generate FCB or save configuration

User interface overview

Main interface components

Welcome Panel

The Welcome Panel is located in the top-right corner of the interface and serves as the starting point for toolchain management and initial setup. It provides access to options such as installing and managing the toolchain, allowing users to configure their development environment. Through this panel, it is possible execute commands to install the toolchain, uninstall it if needed, and check for available updates to ensure the setup remains current and functional.

Device selection panel (MCU & Memory)

This panel is located at the top of the interface, making it easily accessible as the starting point for configuration. The panel allows choosing the target microcontroller unit (MCU) and the memory chip you intend to work with. This selection is essential for tailoring the configuration and generation process to your specific hardware setup. Currently, the RT1180 microcontroller is available for selection. Additional devices will be supported in future updates.

Panel sections:

  • MCU Device selection: Choose the microcontroller that matches your project requirements.

  • Memory Chip selection: Select the memory chip that will be paired with the chosen MCU.

  • Import / Save / Generate FCB Buttons: Use these buttons to import existing configurations, save your current setup, or generate the Flash Configuration Block (FCB) based on your selections.

Configuration panel

The Configuration Panel is located in the center area of the interface and is used to set up parameters for serial memory.

Panel sections:

  • Core Configuration

  • Memory Information Configuration

  • FlexSPI connection configuration

  • Memory LUT Configuration

Tests panel

The Tests Panel is located on the right side of the center area and is designed to display validation results and errors. It features validation, providing feedback on the correctness of the configuration, and indicates whether the current setup passes or fails. This helps users identify and resolve issues, ensuring an accurate configuration process.

Connection panel

The Connection Panel is located at the bottom right side of the interface and is used to detect whether a development board is connected. It shows the current connection status and allows users to manually refresh the connection by clicking the Refresh connection button. This helps ensure that the system is properly linked to the hardware before proceeding with further configuration or testing.

Troubleshooting

This chapter contains known problems and recommended solutions.

Issue: tool does not start

Symptoms: Extension loads but the tool interface does not appear.

Solutions:

  1. Restart VS Code

  2. Check if Python environment is properly installed

  3. Run “Manage Toolchain” and Uninstall current Toolchain

  4. Reinstall Toolchain using “Install Toolchain” button

  5. Check VS Code output panel for error messages

Issue: device is not recognized

Symptoms: RT1180 does not appear in the device list.

Solutions:

  1. Make sure to use a supported Windows version

  2. Update the extension to the latest version

  3. Check system requirements

Known issues and limitations

This chapter contains limitations and possible workaround.

Current limitations

  1. Operating system support:

  • Currently supported only on Windows 10/11 (64-bit)

  • macOS and Linux support is available in future releases

  1. Device support:

  • Limited to RT1180 microcontroller family

  • Additional device support is in development

Workarounds

Unsupported operating systems
  • Use a Windows virtual machine

  • Wait for future OS support updates

Additional device support
  • Check for extension updates regularly

  • Contact NXP support for roadmap information

References

  1. Documentation:

  • RT1180 reference manual

  1. Online resources:

  1. Technical support:

  • NXP Technical Support Portal (link - TBD)

  • Submit issues through the VS Code extension page (link - TBD)

  • Contact your local NXP representative (link - TBD)

Revision history

Document ID

Release date

Description

UG10328 v.2.0

12 December 2025

Updated for 25.12.

UG10328 v.1.0

4 December 2025

Initial version.

Note about the source code in the document

Example code shown in this document has the following copyright and BSD-3-Clause license:

Copyright 2025 NXP Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.

  2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.

  3. Neither the name of the copyright holder nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS “AS IS” AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Disclaimers

Limited warranty and liability — Information in this document is believed to be accurate and reliable. However, NXP Semiconductors does not give any representations or warranties, expressed or implied, as to the accuracy or completeness of such information and shall have no liability for the consequences of use of such information. NXP Semiconductors takes no responsibility for the content in this document if provided by an information source outside of NXP Semiconductors.

In no event shall NXP Semiconductors be liable for any indirect, incidental, punitive, special or consequential damages (including - without limitation - lost profits, lost savings, business interruption, costs related to the removal or replacement of any products or rework charges) whether or not such damages are based on tort (including negligence), warranty, breach of contract or any other legal theory.

Notwithstanding any damages that customer might incur for any reason whatsoever, NXP Semiconductors’ aggregate and cumulative liability towards customer for the products described herein shall be limited in accordance with the Terms and conditions of commercial sale of NXP Semiconductors.

Right to make changes — NXP Semiconductors reserves the right to make changes to information published in this document, including without limitation specifications and product descriptions, at any time and without notice. This document supersedes and replaces all information supplied prior to the publication hereof.

Suitability for use — NXP Semiconductors products are not designed, authorized or warranted to be suitable for use in life support, life-critical or safety-critical systems or equipment, nor in applications where failure or malfunction of an NXP Semiconductors product can reasonably be expected to result in personal injury, death or severe property or environmental damage. NXP Semiconductors and its suppliers accept no liability for inclusion and/or use of NXP Semiconductors products in such equipment or applications and therefore such inclusion and/or use is at the customer’s own risk.

Applications — Applications that are described herein for any of these products are for illustrative purposes only. NXP Semiconductors makes no representation or warranty that such applications will be suitable for the specified use without further testing or modification.

Customers are responsible for the design and operation of their applications and products using NXP Semiconductors products, and NXP Semiconductors accepts no liability for any assistance with applications or customer product design. It is customer’s sole responsibility to determine whether the NXP Semiconductors product is suitable and fit for the customer’s applications and products planned, as well as for the planned application and use of customer’s third party customer(s). Customers should provide appropriate design and operating safeguards to minimize the risks associated with their applications and products.

NXP Semiconductors does not accept any liability related to any default, damage, costs or problem which is based on any weakness or default in the customer’s applications or products, or the application or use by customer’s third party customer(s). Customer is responsible for doing all necessary testing for the customer’s applications and products using NXP Semiconductors products in order to avoid a default of the applications and the products or of the application or use by customer’s third party customer(s). NXP does not accept any liability in this respect.

Terms and conditions of commercial sale — NXP Semiconductors products are sold subject to the general terms and conditions of commercial sale, as published at https://www.nxp.com/profile/terms, unless otherwise agreed in a valid written individual agreement. In case an individual agreement is concluded only the terms and conditions of the respective agreement shall apply. NXP Semiconductors hereby expressly objects to applying the customer’s general terms and conditions with regard to the purchase of NXP Semiconductors products by customer.

Export control — This document as well as the item(s) described herein may be subject to export control regulations. Export might require a prior authorization from competent authorities.

Suitability for use in non-automotive qualified products — Unless this document expressly states that this specific NXP Semiconductors product is automotive qualified, the product is not suitable for automotive use. It is neither qualified nor tested in accordance with automotive testing or application requirements. NXP Semiconductors accepts no liability for inclusion and/or use of non-automotive qualified products in automotive equipment or applications.

In the event that customer uses the product for design-in and use in automotive applications to automotive specifications and standards, customer (a) shall use the product without NXP Semiconductors’ warranty of the product for such automotive applications, use and specifications, and (b) whenever customer uses the product for automotive applications beyond NXP Semiconductors’ specifications such use shall be solely at customer’s own risk, and (c) customer fully indemnifies NXP Semiconductors for any liability, damages or failed product claims resulting from customer design and use of the product for automotive applications beyond NXP Semiconductors’ standard warranty and NXP Semiconductors’ product specifications.

HTML publications — An HTML version, if available, of this document is provided as a courtesy. Definitive information is contained in the applicable document in PDF format. If there is a discrepancy between the HTML document and the PDF document, the PDF document has priority.

Translations — A non-English (translated) version of a document, including the legal information in that document, is for reference only. The English version shall prevail in case of any discrepancy between the translated and English versions.

Security — Customer understands that all NXP products may be subject to unidentified vulnerabilities or may support established security standards or specifications with known limitations. Customer is responsible for the design and operation of its applications and products throughout their lifecycles to reduce the effect of these vulnerabilities on customer’s applications and products. Customer’s responsibility also extends to other open and/or proprietary technologies supported by NXP products for use in customer’s applications. NXP accepts no liability for any vulnerability. Customer should regularly check security updates from NXP and follow up appropriately.

Customer shall select products with security features that best meet rules, regulations, and standards of the intended application and make the ultimate design decisions regarding its products and is solely responsible for compliance with all legal, regulatory, and security related requirements concerning its products, regardless of any information or support that may be provided by NXP.

NXP has a Product Security Incident Response Team (PSIRT) (reachable at PSIRT@nxp.com) that manages the investigation, reporting, and solution release to security vulnerabilities of NXP products.

NXP B.V. — NXP B.V. is not an operating company and it does not distribute or sell products.

Trademarks

Notice: All referenced brands, product names, service names, and trademarks are the property of their respective owners.

NXP — wordmark and logo are trademarks of NXP B.V.