Explore Extension

The NXP MCUXpresso for Visual Studio Code (VS Code) extension can be easily enabled by selecting the MCUXpresso for VS Code icon from the toolbar on the left side. This will open a view that contains the main contributions of the extension, including Quickstart Panel, Imported Repositories, Projects, Debug Probes, Device Tree, Image Info.

MCUXpresso for VS Code

Note: You can use shortcut key (Alt-X for Windows and Linux / ⌘-X for macOS) to return to MCUXpresso view from anywhere inside Visual Studio Code .

Quickstart Panel

Expanding the QUICKSTART PANEL view will display quick links to important components of the extension, including:

  • Shortcut to add a new software repository from a remote server, local archive file, or local folder;

  • Shortcuts to add or create a project by importing it from an existing source repository, an existing project, an archived project or an executable file;

  • Shortcut to NXP Application Code Hub, a repository with software examples, code snippets, application software packs and demos for microcontroller applications.

  • Link to open MCUXpresso Installer

  • Link to online documentation (this documentation).

Toolbar of the QUICKSTART PANEL also provides quick access to the following:

  • Online documentation.

  • MCUXpresso for VS Code walktrough (an organized tour that familiarizes new users with the installation and features of the extension).

  • Issue reporter.

  • Flash Programmer tool.

MCUXpresso for VS Code

Imported Repositories

This area shows the user all imported source repositories. This includes MCUXpresso SDK, Zephyr, Matter and/or Application Code Hub repositories. Multiple instances of each can be handled by this view. Each repository can be expanded to provide details on the imported version.

Imported Repositories

Projects

This is the equivalent of a workspace area, containing settings and details about all MCUXpresso projects that the user has loaded or created. Each project entry will contain project details:

  • Settings - list of configuration files present under .vscode folder.

    • c_cpp_properties.json - C/C++ IntelliSense configuration for the current project.

    • launch.json - debug configurations for the current project.

    • mcuxpresso-tools.json - settings for MCUXpresso for VS Code extension.

    • settings.json - VS Code settings that apply to current workspace folder.

    • tasks.json - file consumed by the task system from VS Code. MCUXpresso for VS Code extension inserts CMake tasks for building, configuring and cleaning projects.

    • CMakePresets.json - description of the CMake Presets.

  • MCU - hardware reference elements of the target like board, device, core, device package. repository.

  • Domains - list of available domains for multi-core devices.

  • Build Configurations - list of available build configurations.

  • Debug Configurations - list of available MCUXpresso-specific debug configurations.

  • Repository - link to the software repository that is used in conjunction with the project.

  • Project Files - link to the project dicrectory.

Note: Source files are available in the Explorer view within VS Code. A user can switch between the project and source views by selecting the desired project and pressing the “Go to Explorer” button in that project’s toolbar.

File Explorer

Debug Probes

All connected and identified debug probes will be listed here. Debug probes can be associated with projects. Go to the Debug section for more details.

Debug Probes

Device Tree

Provides a viewer for device tree system files used in the context of Zephyr development. Go to the Devicetree section for more details.

Device Tree

Image Info

Provides a binary image analysis consisting of a static function callgraph, memory usage and memory content. Go to the Image Info section for more details.

Image Info