Zephyr Lab MCXN947 Kconfig

Objectives

In this lab, you will learn:

  • How to verify Kconfig settings for a Zephyr application

  • How to modify Kconfigs for an application

  • How to open the guiconfig tool, and explore or search for Kconfig settings and details

  • How to create board-specific Kconfig files in an application

  • How to change the compiler optimization Kconfigs

  • How to increase Kconfigs for stack sizes

Kconfig Lab

The software used to build Zephyr applications can be configured at build time to adapt for specific application and platform needs. Configuration is handled through Kernel Config (Kconfig), which is the same configuration system used by the Linux kernel. The goal is to support configuration without having to change any source code.

Configuration options (often called symbols) are defined in Kconfig files, which also specify dependencies between symbols that determine what configurations are valid. Kconfig definitions and settings come from many sources in the Zephyr tree, including:

The outputs from Kconfig are build-time generated files for the application. One text file .config is the final merged Kconfig symbols from all Kconfig sources used by the application. Another file autoconf.h is a C header file with macros that can be tested at build time. These lab steps will demonstrate how these files are useful, to confirm the Kconfig settings used during the most recent build of the application.

Kconfigs can be defined as different types. In this lab, we will explore 3 different types: boolean, integer, and choice Kconfigs. The lab steps will modify the following Kconfigs, and demonstrate how they configure the application:

  • CONFIG_CONSOLE : (type boolean) selects if Zephyr’s Console subsystem is included in the application

  • CONFIG_COMPILER_OPTIMIZATIONS : (type choice) selects which compiler optimization setting is used when the application is built

  • CONFIG_MAIN_STACK_SIZE : (type integer) sets the stack size in bytes for the Main thread

For Zephyr application development, typically Kconfig options are set at the application level. This lab will give some simple examples to get familiar with how Kconfigs are modified for applications. These lab sections include modifying the prj.conf file, which is the Kconfig file at the application level. And also create a new board-specific Kconfig file, which configures the app when it is built for a specific board.

1. Changing a Kconfig symbol for an application

First we will import a Zephyr sample application into VS Code, build it, explore the existing Kconfig symbols, and make a simple Kconfig change. This section uses the blinky application, and will modify the application Kconfig in prj.conf.

  1. Open VS Code. In the Quickstart Panel, click Import Example from Repository. If needed, the steps to import an example, build, and debug it are included in Zephyr Lab MCXN947 Hello World.

    Import Zephyr Example

  2. Import the Blinky Sample with the following settings:

    • For the board, you can type n947 to filter the board target frdm_mcxn947/mcxn947/cpu0. Be sure this board target ends with cpu0.

    • For the example template, type blinky to filter the app zephyr/samples/basic/blinky

    • For Application type, select Repository Application

    • For Zephyr SDK, choose Use recommended version (1.0.1)

    • Click Import

      Import Blinky Example

  3. Build the blinky project

    Build Blinky Example

  4. If not already connected to the board, connect the USB Type-C cable to J17, to power and debug the board. In VS Code, connect the Serial Monitor to the board’s COM port, and click Start Monitoring.

    Connect Serial Monitor

  5. When the build completes, take note of the memory sizes. We will refer back to this memory usage in the later steps in this lab. In VS Code, this is found in the Terminal view after the build completes.

    Blinky memory usage

  6. Debug the blinky project.

    Debug Blinky Example

  7. In the Serial Monitor view, you will see the app prints the boot banner during the startup code, before main() is reached. It also prints the Zephyr version used during the build:

    Blinky boot banner in Serial Monitor:

    *** Booting Zephyr OS build v4.4.0 ***
    
  8. Continue executing the application. The red LED D2 should be blinking.

    Continue debugging

  9. Stop the debugger

    Stop debugger

    Now that we have the default blinky sample working, we will explore some Kconfig settings, and make some simple changes.

  10. In the Explorer view, find the debug folder under the blinky project. This is a generated folder created when building the blinky project. It contains all the generated files from the build tools, like the object code from the compiler, and the linker outputs. In the debug folder, open the file zephyr/.config.

    Blinky build folder

The .config file is the final merged Kconfig settings for the application, generated when the application is built. It is a helpful resource to use to confirm the Kconfig settings used by the application. The Kconfig settings can come from many different source files during the build. They can also have dependencies on other Kconfigs. Sometimes a Kconfig setting can be confusing when reviewing the sources. Verifying the Kconfig in the .config file confirms the setting used during the build. And these lab steps demonstrate, after making Kconfig changes, it is helpful to review the generated .config file to confirm those changes were used during the build.

Another good tip is to review the .config file to optimize your application. You may find there are features, drivers or subsystems enabled that you do not need in your application, and you can make changes to remove them. Or the .config file may reveal settings that are not ideal for your application, and you can change them.

Because the .config file is generated during the build, it is important to understand what happens when changing this file. Any modifications to this file can be reverted if the .config file is re-generated again during a build. For Kconfig changes to be retained, it is best to make the change in a Kconfig source file. In this lab section, we will demonstrate modifying the application’s prj.conf file, and then confirming the modification in the .config file.

  1. In the .config file, search for the symbol CONFIG_CONSOLE. This is a boolean Kconfig, and shows as “=y”. Booleans use y for Yes and n for No. Here “=y” means the symbol is selected, or enabled. Symbols that are not selected (or disabled) are commented out. In this example .config file below, we see that CONFIG_CONSOLE is selected by default in the blinky sample, and CONFIG_SOC_EARLY_INIT_HOOK is not selected.

    # CONFIG_SOC_EARLY_INIT_HOOK is not set
    CONFIG_CONSOLE=y
    
  2. In the Explorer view, open the prj.conf file under the blinky project.

    Open prj.conf file

  3. Modify the prj.conf file, by adding the line highlighted below for CONFIG_CONSOLE. This will disable the Console subsystem, and it will be removed from the application. Save the prj.conf file (Ctrl-S)

    CONFIG_GPIO=y
    
    CONFIG_CONSOLE=n # Add this line
    

    Notice after saving this file, the build tools are run immediately. It does not build the application image or run the C compiler. But it does run the Kconfig tools, and re-generates the .config file with this change.

  4. Go back to the .config file already open in the editor. Notice that CONFIG_CONSOLE is no longer set in this generated file.

    # CONFIG_CONSOLE is not set
    
  5. Go back to the MCUXpresso for VSCode perspective, then Rebuild the blinky application. When the build finishes, the memory usage in the Output view shows a slight reduction in the flash size, since the Console subsystem has been removed from the application:

    Open prj.conf file

    CONFIG_CONSOLE = y

    Memory region

    Size

    % Used

    FLASH:

    26712 B

    1.27%

    RAM:

    4448 B

    1.36%

    CONFIG_CONSOLE = n

    Memory region

    Size

    % Used

    FLASH:

    26588 B

    1.27%

    RAM:

    4448 B

    1.36%


  1. If you debug the blinky application now with the Serial Monitor connected, you will find the app no longer prints the boot banner with the Console removed. You can see the application still executes correctly with the LED blinking.

2. guiconfig tool to explore Kconfig symbols

In this section, we will introduce a tool integrated with Zephyr called guiconfig. This is an interactive tool to explore and configure Kconfig symbols. Guiconfig can be helpful to search for Kconfig symbols, see the different options, understand the dependencies with other symbols, and find where the symbols are located in the source files.

Zephyr offers two similar tools for this, the other is called menuconfig. The difference is menuconfig is text-based for CLI, while guiconfig opens a new window and works with the mouse. The MCUXpresso extension enables opening guiconfig for a project directly in VS Code.

  1. In VS Code, return to the .config file already opened in the editor.

  2. Search (CTRL + F) for the word OPTIMIZATIONS. You will find these symbols:

    CONFIG_SIZE_OPTIMIZATIONS=y
    # CONFIG_SIZE_OPTIMIZATIONS_AGGRESSIVE is not set
    # CONFIG_SPEED_OPTIMIZATIONS is not set
    # CONFIG_DEBUG_OPTIMIZATIONS is not set
    # CONFIG_NO_OPTIMIZATIONS is not set
    

These Kconfig symbols are for the compiler optimizations. When debugging an application and stepping through code, it is helpful to disable optimizations. You can see Zephyr offers an optimization setting for debugging. But we prefer to disable all optimizations when single-stepping or setting breakpoints.

But how does one find that these Kconfigs exist, or how to use them? One option we will use for this is guiconfig.

  1. To open guiconfig, click the MCUXpresso view, Right-Click the blinky project, and select Open Kconfig GUI Configuration.

    Open guiconfig

VS Code needs some time to open the tool. Then the guiconfig window will open.

Guiconfig window

  1. Check the “Show name” box. This adds a column on the right with the name of the Kconfig symbols.

    Check "Show name" box

  2. To search for a Kconfig symbol, click the Jump to button.

    Jump to button

  3. Search for the word OPTIMIZATIONS. The results below are found.

    OPTIMIZATIONS results

  4. To see a more intuitive view, double-click on the “optimize for size” result; or click “optimize for size” then click “Jump to selected item”.

    optimize for size

Guiconfig helps illustrate that Kconfigs are like a hierarchical menu. You can use guiconfig (or menuconfig) to browse through the menu to find all the Kconfig settings, and make changes. We also see here the OPTIMIZATIONS setting is a choice Kconfig. Guiconfig uses a radio button for this choice, to pick 1 of the 4 options. The text in the lower window shows details about each symbol, like a description, and the source where this Kconfig is defined.

  1. Click the setting Optimize nothing to disable compiler optimizations, then click the Save button, and close the guiconfig window.

    Save "Optimize nothing"

  2. Back in VS Code, return to the .config file already open in the editor. Notice guiconfig made changes to the OPTIMIZATIONS settings. We saw in guiconfig, this OPTIMIZATIONS Kconfig is a choice of 4 options. But to select a choice, we select the boolean CONFIG_NO_OPTIMIZATIONS=y, which also deselected CONFIG_SIZE_OPTIMIZATIONS.

    # CONFIG_SIZE_OPTIMIZATIONS is not set
    # CONFIG_SIZE_OPTIMIZATIONS_AGGRESSIVE is not set
    # CONFIG_SPEED_OPTIMIZATIONS is not set
    # CONFIG_DEBUG_OPTIMIZATIONS is not set
    CONFIG_NO_OPTIMIZATIONS=y
    

Guiconfig made this change in the .config file. But remember, this is a generated file, and will not retain this change if it is rebuilt. We could build the app with this change right now, and see the change’s effect on the app. But to make this change permanent, we should add this Kconfig selection to our app’s prj.conf file.

  1. Return to the prj.conf file already open in the editor. Add the highlighted line below for CONFIG_NO_OPTIMIZATIONS, and save the file.

    CONFIG_GPIO=y
    CONFIG_CONSOLE=n
    
    CONFIG_NO_OPTIMIZATIONS=y # Add this line
    
  2. In the MCUXpresso view, rebuild the blinky application. At the end of the build, the memory usage shows a large increase in flash usage after optimizations are disabled. But this change can also make the app much easier to debug.

    CONFIG_SIZE_OPTIMIZATIONS=y

    Memory region

    Size

    %age Used

    FLASH:

    26588 B

    1.27%

    RAM:

    4448 B

    1.36%

    CONFIG_NO_OPTIMIZATIONS=y

    Memory region

    Used Size

    %age Used

    FLASH:

    51548 B

    2.46%

    RAM:

    4504 B

    1.37%

3. Board-specific Kconfigs for an application

The previous sections set application Kconfigs using the app’s prj.conf file. Kconfigs in the prj.conf apply across any hardware platform that app is built on. Another option is to create a board-specific Kconfig file for the application. This is useful when you want the same application to build on multiple boards, and may want different Kconfigs depending on the hardware. This method is frequently used by the sample applications in the Zephyr repository, like tests/drivers/i2s/i2s_speed/board/frdm_mcxn947_mcxn947_cpu0.conf. This lab section will give an example of setting board-specific Kconfigs for an app.

In the last section, the lab steps disabled compiler optimizations to ease debugging. A common consequence of disabling optimizations for an application is that a stack size may need to increase to enable the larger RAM requirement. These steps will first intentionally overflow the existing stack size for the Main thread, and then increase the Main thread stack size using CONFIG_MAIN_STACK_SIZE. Other stack size settings frequently used in Zephyr applications include:

  • CONFIG_IDLE_STACK_SIZE

  • CONFIG_ISR_STACK_SIZE

  • Plus each thread has an individual stack size

For the first steps, we will confirm the current CONFIG_MAIN_STACK_SIZE. And then intentionally overflow this stack size.

  1. In VS Code, return to the .config file already open in the editor. Search for CONFIG_MAIN_STACK_SIZE, and take note of the current size. This is an example of an integer Kconfig, setting the size in bytes:

    CONFIG_MAIN_STACK_SIZE=1024
    
  2. In the Explorer view, open main.c, in the src folder.

    Open main.c

  3. To overflow the Main thread stack, copy and add the middle section of code below, and add to the beginning of main() in main.c. To overflow the stack, we are declaring an array that is size 1+CONFIG_MAIN_STACK_SIZE. Save main.c (Ctrl-S).

    int main(void)
    {
            int ret;
            bool led_state = true;
    
            /*---- Add an array that is too large for the Main thread stack ------*/
            uint8_t large_buf[1025] = {0};
            if(large_buf[0] != 0)    
                    while(1);
            /*-------------------- and force it's compilation --------------------*/
    
            if (!gpio_is_ready_dt(&led)) {
                    return 0;
            }
    
  4. Optional, if you build and debug the application now, you will find the app builds, but it no longer blinks the LED, and instead ends up in a fault when the stack overflows. Optional debug stack overflow

The next steps will increase the size of CONFIG_MAIN_STACK_SIZE, using a board-specific Kconfig file.

  1. In the Explorer view, right-click the boards folder under the blinky project, and select New File. New kconfig file

  2. The new file must be named after the board target we are building for: frdm_mcxn947_mcxn947_cpu0.conf

    New file frdm_mcxn947_mcxn947_cpu0.conf

  3. Copy the line below, and add to the new file. Save frdm_mcxn947_mcxn947_cpu0.conf (Ctrl-S)

    CONFIG_MAIN_STACK_SIZE=2560
    
  4. Back in the MCUXpresso extension, force a Pristine Build. Note that asking VS Code to do a normal build will not work. The build system will not detect that a new Kconfig file was added to the application, so it will think nothing has changed since the last build. To force the build system to include the new file, go to the MCUXpresso view, right-click the blinky project, and select Pristine Build.

    Clean project

  5. Build the blinky project, processes all the Kconfigs, and re-generated the .config file. If you return to .config already open in the Editor, CONFIG_MAIN_STACK_SIZE has been updated to 2560.

  6. Debug the blinky project, and run on the board. The LED blinks again, now with the larger Main thread stack size.

4. Clean up after lab

This Kconfig lab is completed. But the following steps will clean up the VS Code workspace:

  1. Stop the Debugger

    Stop debugger

  2. Close all Editor tabs. Right-Click on a tab, and select Close All.

    Close All Editor Tabs

  3. If this is the last lab and you are done using the board, you should disconnect the Serial Monitor. Find the Serial Monitor view, and click Stop Monitoring.

    Stop Serial Monitor

Additional Resources


Lab completed. Return to the MCXN947 Zephyr Labs Overview Training Zephyr Getting Started MCXN947