Installation
This chapter describes the procedure required to install SEC on Windows, macOS, and Linux operating systems. For the supported operating systems, refer to
Minimum system requirements
The tool runs on Microsoft(R) Windows(R), Ubuntu, and macOS operating systems. The detailed system requirements are specified in Secure Provisioning Tool Release Notes. The document also describes what debug probe drivers should be installed. These drivers might also be needed for communication with the processor in ISP mode where the probe provides USB to UART/SPI/I2C converter.
Windows
To install SEC as a desktop application on a local host, perform the following steps:
Visit the Secure Provisioning Tool home page to download the SEC installer for Windows.
Double-click the
MCUXpresso_Secure_Provisioning_<version>.exeinstaller to begin installation.On the first page of the wizard, click Next.
Secure Provisioning Tool Setup
On the End-User License Agreement page of the wizard, select I accept the terms of the License Agreement and click Next.
Accepting the end-user license agreement
On the Select Installation Folder page of the wizard, select Browse and navigate to a destination folder you want to install the SEC to and click Next.
Selecting installation folder
On the Configure Shortcuts page of the wizard, select the shortcuts you want to be created for SEC and click Next.
Configuring shortcuts
On the Ready to Install page of the wizard, select Install.
The setup begins the installation.
Note: If you want to review or change any of your installation settings, click Back. Click Cancel to exit the wizard.
The installer prompts you when the installation completes.
Ready to install
Installing Secure Provisioning Tool
Click Finish to close and exit the setup wizard.
Completing installation
To start using SEC, run the tool from the desktop shortcut on the desktop or from the Start menu. You can also navigate to the <product installation folder>\bin\ folder and launch the
securep.exeor launch the shortcut in the <product installation folder>.
Windows CLI
It is possible to install the SEC Tool using the command line. In this case, use Run the installer with the following parameters: start /wait
MCUXpresso_Secure_Provisioning_YY.MM.exe /exenoui /qn
MacOS
To install SEC as a desktop application on a local host, perform the following steps:
Visit the NXP website to download the SEC installer for macOS. Based on your computer, select either an installer for an Intel or Apple M processor.
Double-click the
MCUXpresso_Secure_Provisioning_YY.MM.pkgto start the Install MCUXpresso Secure Provisioning Tool wizard.
Note: When you try to open the macOS installer, you may receive an error. To avoid it, manually select the option Mac App Store and identified developers in the Security & Privacy menu.
On the Introduction page, click Continue.
Introduction
On the Software License Agreement page, click Continue.
Software license agreement
Confirm that you have read and agreed to the terms of the Software License Agreement by clicking Agree.
Accepting software license agreement
On the Destination Select page, click the green arrow to select the installation folder, and once done, click Continue.
Select destination
On the Installation Type page, click Install.
Installation type
Type in your login credentials to continue with the installation and click Install Software.
Install software
Click Continue.
Unless errors are reported, the Summary page confirms that the installation was completed successfully.
On the Summary page, click Close.
Summary
Enabling USB connection on macOS
During the first connection to the target by USB, macOS X Catalina blocks the access to USB HID devices as a security measure and the operation will fail with error. In macOS 13 (Ventura), this works differently and these steps are not needed.
Perform the following steps to enable USB connection:
In the OS security alert message box, select Open System Preferences.
Open System Preferences
Unlock Privacy preferences to enable changes.
Select MCUXpresso Secure Provisioning Tool YY.MM, confirm, and quit the application.
Confirm change
Lock Privacy preferences.
If the application was not closed, close it manually.
Start the application and proceed with the operation.
Linux
Installation of SEC on Ubuntu can be done in the Terminal.
Visit the NXP website to download the SEC installer for Linux.
Open the terminal and change the directory where the installer is downloaded, install using dpkg with sudo.
$ cd ~/Downloads $ sudo dpkg -i mcuxpresso-secure-provisioning-<version>_<architecture>_<os-version>.deb
If the command executed with sudo is successful, the setup installs the SEC Tool in the dedicated folder /opt/nxp/.
Note: SEC depends on other packages that have to be installed in advance:
$ sudo apt install libhidapi-dev libsdl2-2.0-0
Uninstalling
Windows
The Secure Provisioning Tool can be uninstalled in the following ways:
MacOS
Secure Provisioning Tool can be uninstalled by using Finder, navigating to Applications, and moving SEC_Provi_##.## into the Trash.
Linux
The Secure Provisioning Tool can be uninstalled by using the Debian package manager.
In the Terminal you can get the list of secure provisioning tools with the package names:
$ dpkg --list "*-secure-provisioning*"
Desired=Unknown/Install/Remove/Purge/Hold
| Status=Not/Inst/Conf-files/Unpacked/halF-conf/Half-inst/trig-aWait/Trig-pend
|/ Err?=(none)/Reinst-required (Status,Err: uppercase=bad)
||/ Name Version Architecture Description
+++-=======================================-============-============-====================================
ii mcuxpresso-secure-provisioning-25.09 25.09 amd64 MCUXpresso Secure Provisioning Tool
ii mcuxpresso-secure-provisioning-v3.1 3.1 amd64 MCUXpresso Secure Provisioning
ii mcuxpresso-secure-provisioning-v4 4.0 amd64 MCUXpresso Secure Provisioning
Now, the desired version can be uninstalled:
$ sudo dpkg --remove mcuxpresso-secure-provisioning-25.09
Remove configuration files
The user preferences are stored in the folder <user home>\.nxp\secure_provisioning_<version>\ and are not removed by uninstalling the product. These folders can be removed manually. For more details about preferences, see Preferences.
Remove restricted data
The restricted data are installed in the folder <user home>\.nxp\secure_provisioning_restricted_data\ and are not removed by uninstalling the product. These folders can be removed manually.