MCUXpresso SDK Documentation

Build Targets#

The RT2660 SDK provides seven build targets across two categories: five Unified Linkage targets and two RAM ONLY targets.

For all debug sessions, set the MIMXRT2660-EVK boot switch to 0b00 (XSPI NOR boot mode).

Quick reference#

Target

Type

POR boot

debug

Unified Linkage

Yes – XSPI NOR flash

xspi_nor

Unified Linkage

Yes – XSPI NOR flash

xspi_nor_psram

Unified Linkage

Yes – XSPI NOR flash

psram

Unified Linkage

Yes – XSPI NOR flash

psram_txt

Unified Linkage

Yes – XSPI NOR flash

ram_only

RAM ONLY

Yes – eMMC or XSPI NOR flash (requires boot header)

psram_only

RAM ONLY

Yes – eMMC or XSPI NOR flash (requires boot header)

Note: the default SDK build for ram_only and psram_only does not include a boot header and cannot POR boot.


Unified Linkage targets#

Unified Linkage is the mainstream linkage approach for MIMXRT2660-EVK SDK examples.

The five Unified Linkage targets all boot from XSPI NOR flash. The image is programmed into flash, startup runs XIP from flash, then code is copied (or left in flash) according to the target before jumping to main().

Coming from legacy RT1xxx? Although some target names look familiar (e.g. debug, psram), the Unified Linkage mechanism on RT2660 is fundamentally different from the legacy RT1xxx RAM-download flow. Do not assume the same debug behavior – read this guide before proceeding.


RAM ONLY targets#

The two RAM ONLY targets (ram_only and psram_only) do not use XSPI NOR flash as part of the debug flow.

The default build for both targets does not include a USDHC boot header.

The standard workflow is download to RAM then run: the debugger connects, downloads the ELF directly into ITCM or PSRAM, and starts execution – no flash programming required, which makes the iteration cycle faster.

RAM ONLY images are volatile: cycling power clears the program.

Coming from legacy RT1xxx? These two targets are the closest equivalent to the legacy RAM-download flow: ram_only corresponds to debug on RT1xxx (code in TCM), and psram_only corresponds to psram_txt on RT1xxx (code in external RAM).

One-time preparation required for psram_only: a one-time board setup step is required before the first debug session.