ZPS_eAplZdpMgmtLqiRequest
ZPS_teStatus ZPS_eAplZdpMgmtLqiRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpMgmtLqiReq *psZdpMgmtLqiReq);
Description
This function requests a remote node to provide a list of neighboring nodes, from its Neighbor table, including LQI (link quality) values for radio transmissions from each of these nodes. The destination node of this request must be a Router or the Co- ordinator.
This request must specify the index of the first node in the Neighbor table to report. The request is represented by the structure below (further detailed in Section 8.2.2.34).
typedef struct {
uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtLqiReq;
The remote node replies with a Mgmt_Lqi_rsp response containing the required information, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtLqiRsp(detailed in Section 8.2.3.34).
Parent topic:ZPS_eAplZdpMgmtLqiRequest
Parameters
hAPduInst Handle of APDU instance in which request is sent.
uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpMgmtLqiReq Pointer to request (see above)
Parent topic:ZPS_eAplZdpMgmtLqiRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpMgmtLqiRequest
Parent topic:Network Management Services functions