ZPS_tsAplZdpMgmtLqiRsp
This structure is used to store Mgmt_Lqi_rsp message data - a response to a call to the function ZPS_eAplZdpMgmtLqiRequest(). This response reports a list of neighboring nodes along with their LQI (link quality) values.
The ZPS_tsAplZdpMgmtLqiRspstructure is detailed below.
typedef struct {
uint8 u8Status;
uint8 u8NeighborTableEntries;
uint8 u8StartIndex;
uint8 u8NeighborTableListCount;
/* Rest of the message is variable length */
ZPS_tsAplZdpNtListEntry* pNetworkTableList;
} ZPS_tsAplZdpMgmtLqiRsp;
where:
u8Statusis the return status for ZPS_eAplZdpMgmtLqiRequest()u8NeighborTableEntriesis the total number of Neighbor table entries on the remote nodeu8StartIndexis the Neighbor table index of the first entry reported in this response (throughpNetworkTableList)u8NetworkListCountis the number of Neighbor table entries reported in this response (throughpNetworkTableList)pNetworkTableListis a pointer to the first entry in the list of reported Neighbor table entries. Each entry is of the typeZPS_tsAplZdpNtListEntrydetailed below.ZPS_tsAplZdpNtListEntry
typedef struct { uint64 u64ExtPanId; uint64 u64ExtendedAddress; uint16 u16NwkAddr; uint8 u8LinkQuality; uint8 u8Depth; /* * Bitfields are used for syntactic neatness and space saving. * May need to assess whether these are suitable for embedded environment and may need to watch endianness on u8Assignment */ union { struct { unsigned u1Reserved1:1; unsigned u2Relationship:3; unsigned u2RxOnWhenIdle:2; unsigned u2DeviceType:2; unsigned u6Reserved2:6; unsigned u2PermitJoining:2; } ; uint8 au8Field[2]; } uAncAttrs; } ZPS_tsAplZdpNtListEntry;
where:
u64ExtPanIdis the 64-bit extended PAN ID of the network .u64ExtendedAddressis the IEEE address of the neighboring node.u16NwkAddris the network address of the neighboring node.u8LinkQualityis the estimated LQI (link quality) value for radio transmissions from the neighboring node.u8Depthis the tree depth of the neighboring node (where the Coordinator is at depth zero).u1Reserved1:1is a 1-bit reserved value and should be set zero.u2Relationship:3is a 3-bit value representing the neighboring node’s relationship to the local node:0: Neighbor is the parent.
1: Neighbor is a child.
2: Neighbor is a sibling (has same parent).
3: None of the above.
4: Neighbor is a former child.
u2RxOnWhenIdle:2is a 2-bit value indicating whether the neighboring node’s receiver is enable during idle periods:0: Receiver off when idle (sleeping device)
1: Receiver on when idle (non-sleeping device)
2: Unknown
u2DeviceType:2is a 2-bit value representing the ZigBee device type of the neighboring node:0: Coordinator
1: Router
2: End Device
3: Unknown
u6Reserved2:6is a 6-bit reserved value and should be set zero.u2PermitJoining:2is a 2-bit value indicating whether the neighboring node is accepting joining requests:0: Not accepting join requests
1: Accepting join requests
2: Unknown
au8Field[2]is the allocation of two bytes for the union.
Parent topic:ZDP response structures