MAC codes
The MAC codes come from the IEEE 802.15.4 MAC layer of the stack. The MAC codes may be returned by any ZigBee PRO API function with a non-void return. The codes are also described in the IEEE 802.15.4 Stack User Guide (JN-UG-3024).
MAC codes
Name |
Value |
Description |
|---|---|---|
MAC_ENUM_SUCCESS |
0x00 |
Success |
MAC_ENUM_BEACON_LOSS |
0xE0 |
Beacon loss after synchronization request |
MAC_ENUM_CHANNEL_ACCESS_FAILURE |
0xE1 |
CSMA/CA channel access failure |
MAC_ENUM_DENIED |
0xE2 |
GTS request denied |
MAC_ENUM_DISABLE_TRX_FAILURE |
0xE3 |
Could not disable transmit or receive |
MAC_ENUM_FAILED_SECURITY_CHECK |
0xE4 |
Incoming frame failed security check |
MAC_ENUM_FRAME_TOO_LONG |
0xE5 |
Frame too long, after security processing, to be sent |
MAC_ENUM_INVALID_GTS |
0xE6 |
GTS transmission failed |
MAC_ENUM_INVALID_HANDLE |
0xE7 |
Purge request failed to find entry in queue |
MAC_ENUM_INVALID_PARAMETER |
0xE8 |
Out-of-range parameter in function |
MAC_ENUM_NO_ACK |
0xE9 |
No acknowledgment received when expected |
MAC_ENUM_NO_BEACON |
0xEA |
Scan failed to find any beacons |
MAC_ENUM_NO_DATA |
0xEB |
No response data after a data request |
MAC_ENUM_NO_SHORT_ADDRESS |
0xEC |
No allocated network (short) address for operation |
MAC_ENUM_OUT_OF_CAP |
0xED |
Receiver-enable request could not be executed, as CAP finished |
MAC_ENUM_PAN_ID_CONFLICT |
0xEE |
PAN ID conflict has been detected |
MAC_ENUM_REALIGNMENT |
0xEF |
Coordinator realignment has been received |
MAC_ENUM_TRANSACTION_EXPIRED |
0xF0 |
Pending transaction has expired and data discarded |
MAC_ENUM_TRANSACTION_OVERFLOW |
0xF1 |
No capacity to store transaction |
MAC_ENUM_TX_ACTIVE |
0xF2 |
Receiver-enable request could not be executed, as in transmit state |
MAC_ENUM_UNAVAILABLE_KEY |
0xF3 |
Appropriate key is not available in ACL |
MAC_ENUM_UNSUPPORTED_ATTRIBUTE |
0xF4 |
PIB Set/Get on unsupported attribute |
Parent topic:Return/Status Codes