How to determine COM port
This section describes the steps to determine the debug COM port number of your NXP hardware development platform.
Linux: The serial port can be determined by running the following command after the USB Serial is connected to the host:
$ dmesg | grep "ttyUSB" [503175.307873] usb 3-12: cp210x converter now attached to ttyUSB0 [503175.309372] usb 3-12: cp210x converter now attached to ttyUSB1
There are two ports, one is Cortex-A core debug console and the other is for Cortex M33.
Windows: To determine the COM port, open Device Manager. Click the Start menu and type Device Manager in the search bar.
|

|
In the Device Manager, expand the Ports (COM & LPT) section to view the available ports. The COM port names are different for all the NXP boards.
USB-UART interface
|

|