Architecture
Introduction
The MCUXpresso Software Development Kit (SDK) provides comprehensive development solutions designed to help accelerate embedded system development of applications based on MCUs from NXP. The MCUXpresso SDK includes a flexible set of peripheral drivers designed to speed up and simplify development of embedded applications. Along with the peripheral drivers, the MCUXpresso SDK provides an extensive set of example applications covering everything from basic peripheral use cases to full technology demonstrations. The MCUXpresso SDK contains optional RTOS integrations such as FreeRTOS, and various other middleware to support rapid development.
The MCUXpresso SDK architecture is built around the five key components listed below:
CMSIS - Arm Cortex Microcontroller Software Interface Standard Core: Device headers, Math/DSP libraries
Drivers - SoC peripheral configuration and functions
RTOS - Real-time Operating Systems
Middleware - Compatible Stacks and technology enablement
Applications - Demo and driver examples based on the MCUXpresso SDK

MCUXpresso SDK provides a powerful and robust build and configuration system which covers all aspects of the software development.
CMSIS Support
The MCUXpresso SDK CMSIS folder provides NXP support for the Arm CMSIS Core standard. Along with SoC and peripheral header files, the SDK also includes common CMSIS header files for the Arm Cortex-M cores and the math and DSP libraries. The CMSIS DSP library source code is included for reference.
SoC Support - Header File/Drivers/Startup/Linker…
The MCUXpresso SDK Device folder allows support for multiple devices in the same package. For example, MIMXRT1052 is one of the devices in the RT105X family. The support files required to develop with this device will be in a unique folder inside the devices folder. The following sections detail the content provided in these SoC files:
MCU header files
Each device supported in the MCUXpresso SDK has an overall System-on Chip (SoC) memory-mapped header file. This header file contains the memory map and register base address for each peripheral and the IRQ vector table with the associated vector numbers. The overall SoC header file provides access to the peripheral registers through pointers and predefined bit masks.
The MCU Header file is located in:
devices/<DEVICE_PLATFORM>/<DEVICE_FAMILY\>/<DEVICE_NAME>/<DEVICE_NAME>.h
Feature Header Files
In addition to the overall SoC memory-mapped header file, the MCUXpresso SDK includes a feature header file for each device. The feature header file allows NXP to deliver a single software driver for a given peripheral. The feature file ensures that the driver is properly compiled for the target SOC.
The peripheral drivers are designed to be reusable regardless of the peripheral functional differences from one MCU device to another. An overall Peripheral Feature Header File is provided for the MCUXpresso SDK-supported MCU device to define the features or configuration differences for each sub-family device.
Startup codes
The Startup code file provides the startup functions and assembly code required for the SoC to run from power-Up to the main() function. The code usually covers the stack setup, watchdog configuration, and handles global variables.
The Startup code files are located in:
devices/\<DEVICE_NAME\>/system\_\<DEVICE_NAME\>.c/h
devices/\<DEVICE_NAME\>/\<TOOLCHAIN\>/startup\_\<DEVICE_NAME\>.s/S
Linker files
Linker file are provided for each toolchain. The postfix of the linker file varies from toolchain to toolchain.
The Linker Files are located in:
devices/\<DEVICE_NAME\>/\<TOOLCHAIN\>/\<\>.scf
Peripheral Drivers
The MCUXpresso SDK peripheral drivers mainly consist of low-level functional APIs for the MCU product family on-chip peripherals and also of high-level transactional APIs for some bus drivers/DMA driver/eDMA driver to quickly enable the peripherals and perform transfers.
All MCUXpresso SDK peripheral drivers only depend on the CMSIS headers, device feature files, fsl_common.h, and fsl_clock.h files so that users can add the drivers along with their dependencies into a project.
With the exception of the clock/power-relevant peripherals, each peripheral has its own driver. Peripheral drivers handle the peripheral clock gating/ungating inside the drivers during initialization and deinitialization respectively.
Peripheral Drivers are located in:
devices//\<DEVICE_NAME\>/drivers
Low-level functional APIs provide common peripheral functionality, abstracting the hardware peripheral register accesses into a set of stateless basic functional operations. These APIs primarily focus on the control, configuration, and function of basic peripheral operations. The APIs hide the register access details and various MCU peripheralinstantiation differences so that the application can be abstracted from the low-level hardware details.
The API prototypes are intentionally similar to help ensure easy portability across devices supported in the MCUXpresso SDK.
Transactional APIs provide a quick method for customers to utilize higher-level functionality of the peripherals. The transactional APIs utilize interrupts and perform asynchronous operations without user intervention. Transactional APIs operate on high-level logic that requires data storage for internal operation context handling. However, the Peripheral Drivers do not allocate this memory space. Rather, the user passes in the memory to the driver for internal driver operation.
Transactional APIs ensure the NVIC is enabled properly inside the drivers. The transactional APIs do not meet all customer needs, but provide a baseline for development of custom user APIs.
NOTE The transactional drivers never disable an NVIC after use. This is due to the shared nature of interrupt vectors on devices. It is up to the user to ensure that NVIC interrupts are properly disabled after usage is complete.
Interrupt Handling for Transactional APIs
A double weak mechanism is introduced for drivers with a Transactional API. The double weak indicates two levels of weak vector entries. See the examples below:
PUBWEAK SPI0_IRQHandler
PUBWEAK SPI0_DriverIRQHandler
SPI0_IRQHandler
LDR R0, =SPI0_DriverIRQHandler
BX R0
The first level of the weak implementation are the functions defined in the vector table.
This vector table can be located in:
devices/\<DEVICE_NAME\>/\<TOOLCHAIN\>/startup\_\<DEVICE_NAME\>.s/.S
The implementation of the first layer weak function calls the second layer of weak function. The implementation of the second layer weak function (ex. SPI0_DriverIRQHandler) jumps to itself (B .). The MCUXpresso SDK drivers with transactional APIs provide the reimplementation of the second layer function inside of the peripheral driver. If the MCUXpresso SDK drivers with transactional APIs are linked into the image, the SPI0_DriverIRQHandler is replaced with the function implemented in the MCUXpresso SDK SPI driver.
The reason for implementing the double weak functions is to provide a better user experience when using the transactional APIs. For drivers with a transactional function, call the transactional APIs and the drivers complete the interrupt-driven flow. Users are not required to redefine the vector entries out of the box. At the same time, if users are not satisfied by the second layer weak function implemented in the MCUXpresso SDK drivers, users can redefine the first layer weak function and implement their own interrupt handler functions to suit their implementation.
The limitation of the double weak mechanism is that it cannot be used for peripherals that share the same vector entry. For this use case, redefine the first layer weak function to enable the desired peripheral interrupt functionality. For example, if the MCU’s UART0 and UART1 share the same vector entry, redefine the UART0_UART1_IRQHandler according to the use case requirements.
RTOS Driver
MCUXpresso SDK provides the bus communication driver integrated with native FreeRTOS services. These drivers are called as an RTOS driver and provide the sync transfer APIs. The user can directly call these APIs in FreeRTOS applications.
RTOS drivers are located in same folder of Peripheral Drivers with freertos in the file name. For example:
devices\\MIMXRT1052\\drivers\\fsl_lpi2c_freertos.c/h
CMSIS Driver
MCUXpresso SDK provides CMSIS driver support for all the variants of I2C/UART/SPI peripherals. The MCUXpresso SDK CMSIS driver implementation uses the pin mux configuration APIs generated by the NXP pinmux Config Tool in pinmux.c files.
This is different than the way proposed by ARM to configure the PINMUX configuration by passing a set of macros in RTE_Device.h.
Project Template
See description for Project Template in the Application section found under Development. Compared to a board level project template, device level project templates are for use cases to create a new project for a device different from the one used on a specific board.
Components
SDK provide the components folder in the root directory storing these sensor driver, common software components and so on.
On-Board Device driver
Sensor, PMIC, PHY, Audio Codec which are soldered in the evaluation board will be supported in the SDK. Usually, there drivers can be connected to different variants of the peripheral driver in SoC to make it work. For example, Audio codec can be connected to I2C/LPI2C peripherals.
To ease the porting effort for the same device supporting work with different SoC(Which usually means different variants of peripheral), these device driver will not be implemented bind to specific peripheral like I2C or LPI2C. Instead, it require the application to provide function pointer which is prepared outside of the device driver and device driver can use these APIs to do the data write/read and so on. Device driver don’t care about how these functions pointers are implemented. application can use all variants of way to implement these functions pointer. For example, user can use the CMSIS Driver to implement it or user even can use the raw register read/write to implement it. One important thing to be note here is the initialization/de-initialization of these peripherals will not be done inside the device driver to avoid the race-condition. For example, Audio Codec A and Audio Codec B all use the same I2C. A don’t know the status of B. If A call the de-initialization of I2C, the B’s work may be broken.
Common Software Component
Common software component which are not middleware/stacks will also be placed to this folder. For example, the NAND Flash Component which implement the common NAND flash logic operation. Another example is the application timer. SDK now integrated a lot of stack/middleware inside/outside BL/BU/NXP and some of the middleware/stack provide these kinds of the software components. If certain software component inside these middleware/stack are also requested in other cases, these components will be split out from these middleware/stacks and move to this part if there is no license issue.
Middleware and RTOS
Middle-wares are provided in the directory of middleware folder provided various middleware support.
RTOS are provided in the directory of rtos folder. For FreeRTOS, the bus communication driver are also provided with native FreeRTOS support leveraging services provided by the FreeRTOS. You can find these RTOS drivers from the same location of the peripheral drivers.
RTOS support outside SDK repository
SDK will also support other RTOS but not in the repository of the SDK. Zephyr/Ali-OS/MBED OS are both supported in their community. User can find the support in these public repository.
OSA
SDK don’t provide the unified OSA layers. Middleware needing OSA now get the OSA support inside the middleware.
Application
SDK provide application in boards/<board_name_or_kit_name>/. Board here means the evaluation board created by the NXP avaialbe to customer. Kits here mean a shied board without micro-controller inside. It need work with the evaluation board by connector like Arduino interface. For example, inside the EVKB-IMXRT1050 packages “boards” folder, evkbimxrt1050 is the evaluation board. evkbimxrt1050_agm01 is a shield board which can work with the EVKB-IMXRT1050 board by Arduino connector. AGM01 shield board get multi sensors on the board for user to evaluate NXP sensor product and software.
MCUXpresso SDK board support provides example applications for NXP development and evaluation boards for Arm Cortex-M cores, including Freedom, Tower System, and LPCXpresso boards. Board support packages are found inside of the top level boards folder, and each supported board has its own folder (an MCUXpresso SDK package can support multiple boards). Within each <board_name> folder, there are various sub-folders to classify the type of examples they contain. Except that demo_apps, driver_examples, and cmsis_driver_examples are default for each board, other sub-folders are prepared for each middleware like usb_examples, These include (but are not limited to):
cmsis_driver_examples: Simple applications intended to concisely illustrate how to use CMSIS drivers.
demo_apps: Full-featured applications intended to highlight key functionality and use cases of the target MCU. These applications typically use multiple MCU peripherals and may leverage stacks and middleware.
driver_examples: Simple applications intended to concisely illustrate how to use the MCUXpresso SDK’s peripheral drivers for a single use case. These applications typically only use a single peripheral, but there are cases where multiple are used (for example, SPI conversion using DMA).
emwin_examples: Applications that use the emWin GUI widgets.
rtos_examples: Basic FreeRTOS OS examples showcasing the use of various RTOS objects (semaphores, queues, and so on) and interfacing with the MCUXpresso SDK’s RTOS drivers
usb_examples: Applications that use the USB host/device/OTG stack.
List will be extended with more and more software components integrated into the MCUXpresso SDK
Project Structure
This section describes how the various types of example applications interact with the other components in the MCUXpresso SDK.
Each <board_name> folder in the boards directory contains a comprehensive set of examples that are relevant to that specific piece of hardware. We’ll discuss the hello_world example (part of the demo_apps folder), but the same general rules apply to any type of example in the <board_name> folder.
All files in the application folder are specific to that example, so it is easy to copy and paste an existing example to start developing a custom application based on a project provided in the MCUXpresso SDK.

BOARD specific configuration: board.c/h
board.c/h files are prepared for each board during development. In customer available SDK package, the board.h/c files will be copied to each project. Inside these files, it mainly proivde macros/functions to provide common configuration specific to the board and also that are commonly used by multiple cases. These files are created manually. For example, in the FRDM-K64F board, the UART0 is connected to OPENSDA K20 chips and user can conect to the K20 from PC to get the log input, the board file will debug these UART0 pin connected to OPENSDA K20 as the DEBUG CONSOLE that all cases using debug console needn’t define these macros themselves instead using these macros directly.
Clock configuration : clock_config.c/h
Clock confiugration files are always required to be generated by clock tools in MCUX CFG tools that user can import these files/update files/write back to these files. Clock confiugraiton files provide mutiple clock configuration functions for the application to call. SDK prepare the common clock configuratoin for multiple modes that most of application reuse these files. For some applications with requriement for code size or clock mode, these cases can customize their own clock configuration files accordingly.
PIN configuration: pin_mux.c/h
Pin mux configuration files are always required to be generated by pin tools in MCUX CFG tools that user can import these files/update files/write back to these files. pin mux configuration files are always customized for each applicatiion. pin mux file are create for soc but not for board. If create a pin configuration for a board, a lot of unused functions will be created while it is not needed for specified case.
Project Template
Project template is located in board/<board_name_or_kit_name>/project_template/. Project template are not intented for user’s direct usage. It provide the template for the MCUX CFG tool or CMSIS Pack to create new project as starting point. It provide the basic template of main file, pin mux configuration files, clock configuration files and so on. It existed in board level or soc level. Which file will be used is decided by the request to create proejct for a soc or for a board. There project template need to be updated for each configuration tool update.
boards/<board>/project_tempalate
devices/<soc>/project_template
Build and Configuration System
MCUXpresso SDK build and configuration system is based on CMake and Kconfig. It serves every aspect of the software development:
Toolchain setup
Device enablement
Board enablement
Shield enablement
Component configuration and integration
Example configuration, complication, download and debug
All software data are recorded in cmake, Kconfig and misc yaml files. All functionality commands and arguments have been integrated into MCUXpresso west extension which can be easily used. Please refer Build and Configuration System for more details.
Documentation
Documents are located in docs folder. The Release Notes, Getting Started Guide, API Reference Manual and Change Log document are provided.
Release Notes
Release notes are included with each release of MCUXpresso SDK. It introduces what is delivered in the SDK package and which tools were used to test the package. It also lists any known issues for the release. The MCUXpresso SDK on GitHub delivers support for multiple devices and boards. The Release notes provides a Quality Level for the software support of each device/board. The quality levels are: RFP, EAR, MIN, NON.
Getting Started Guide
A Getting Started Guide is a valuable resource for first evaluation of the MCUXpresso SDK. It describes a clear procedure on how to use the SDK package. It outlines steps to begin working with a typical SDK project. The user will be shown how to compile, program and debug an application for a specific board.
API Reference Manual and Change Log
The API Reference Manual details the API and data structures for a given software component. The content is generated from the doxygen tag in source code.
Change Log is documents describing the changes for software components in the package. They are generated from the doxygen information.