MCUXpresso SDK Release Notes for EVK9-MIMX8ULP
Table of Contents
- Overview
 - MCUXpresso SDK
 - Development tools
 - Supported development systems
 - MCUXpresso SDK release package
 - Release contents
 - MISRA compliance
 - Known issues
- Maximum file path length in Windows 7 operating system
 - Fusion DSP may load wrong data from shared SRAM on Silicon A0.1 with specific command sequence
 - Real-Time Domain cannot normally resume from the power-down mode due to EdgeLock secure enclave (S400) failure
 - Flexcan_ping_pong_buffer_transfer case loses first 8 bytes data for armgcc flash_debug
 - Lpspi_interrupt_b2b_master/slave example transfer fail on iar/armgcc flash target
 - DSP examples build failure in IAR 9.50.1
 - DSP examples cannot boot the Fusion core