Running a Demo Application Using Arm GCC
This section describes the steps to configure the command-line Arm GCC tools to build, run, and debug demo applications. This section also lists the necessary driver libraries provided in the MCUXpresso SDK. The hello_world demo application targeted for the MIMX8ULP hardware platform is used as an example, though these steps can be applied to any board, demo, or example application in the MCUXpresso SDK.
Note: Run an application using imx-mkimage. Generate and download flash.bin to emmc or flexspi nor flash when DBD_EN (Deny By Default) is fused.
Linux OS host
The following sections provide steps to run a demo compiled with Arm GCC on Linux host.
Set up toolchain
This section contains the steps to install the necessary components required to build and run a MCUXpresso SDK demo application with the Arm GCC toolchain, as supported by the MCUXpresso SDK.
Install GCC Arm embedded toolchain
Download and run the installer from the GNU Arm Embedded Toolchain Downloads page. The GNU Arm embedded toolchain contains the GCC compiler, libraries, and other tools required for bare-metal software development. The GCC toolchain should correspond to the latest supported version, as described in the MCUXpresso SDK Release Notes for EVK-MIMX8ULP (document MCUXSDKIMX8ULPRN).
Note: See How to set up Windows/Linux host system for setting up Linux host before compiling the application.
Parent topic:Set up toolchain
Add a new system environment variable for ARMGCC_DIR
Create a new system environment variable and name it ARMGCC_DIR. The value of this variable should point to the Arm GCC embedded toolchain installation path. For this example, the path is:
$ export ARMGCC_DIR=<path_to_GNUARM_GCC_installation_dir>
Parent topic:Set up toolchain
Parent topic:Linux OS host
Build an example application
To build an example application, follow these steps.
Change the directory to the example application project directory, which has a path similar to the following:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgccFor this example, the exact path is:
<install_dir>/boards/evkmimx8ulp/demo_apps/hello_world/armgccRun the
build_debug.shscript at the command-line to perform the build. The output is shown as below:$ ./build_debug.sh -- TOOLCHAIN_DIR: -- BUILD_TYPE: debug -- TOOLCHAIN_DIR: -- BUILD_TYPE: debug -- The ASM compiler identification is GNU -- Found assembler: -- Configuring done -- Generating done -- Build files have been written to: Scanning dependencies of target hello_world.elf < -- skipping lines -- > [100%] Linking C executable debug/hello_world.elf [100%] Built target hello_world.elf
Note: To run the application, see the Run an application using imx-mkimage.
Parent topic:Linux OS host
Parent topic:Running a Demo Application Using Arm GCC
Windows OS host
The following sections provide steps to run a demo compiled with Arm GCC on Windows OS host.
Set up toolchain
This section contains the steps to install the necessary components required to build and run a MCUXpresso SDK demo application with the Arm GCC toolchain on Windows OS, as supported by the MCUXpresso SDK.
Install GCC Arm embedded toolchain
Download and run the installer from the GNU Arm Embedded Toolchain Downloads page. The GNU Arm embedded toolchain contains the GCC compiler, libraries, and other tools required for bare-metal software development. The GCC toolchain should correspond to the latest supported version, as described in MCUXpresso SDK Release Notes for EVK-MIMX8ULP (document MCUXSDKIMX8ULPRN).
Note: See How to set up Windows/Linux host system for setting up Windows host before compiling the application.
Parent topic:Set up toolchain
Add a new system environment variable for ARMGCC_DIR
Create a new system environment variable and name it ARMGCC_DIR. The value of this variable should point to the Arm GCC embedded toolchain installation path. For this example, the path is:
C:\Program Files (x86)\GNU Arm Embedded Toolchain\9 2020-q2-update
Reference the installation folder of the GNU Arm GCC embedded tools for the exact pathname.
Parent topic:Set up toolchain
Parent topic:Windows OS host
Build an example application
To build an example application, follow these steps.
Open the GCC Arm embedded toolchain command window. To launch the window on the Windows operating system, select Start -> Programs -> GNU Tools ARM Embedded <version> -> GCC Command Prompt.
|

|
Change the directory to the example application project directory, which has a path similar to the following:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc
For this example, the exact path is:
<install_dir>/boards/evkmimx8ulp/demo_apps/hello_world/armgcc
Type
build_debug.batat the command-line or double-click thebuild_debug.batfile in Windows Explorer to perform the build. The output is as shown in Figure 2.|

|
Note: To run the application, see the Run an application using imx-mkimage.
Parent topic:Windows OS host
Parent topic:Running a Demo Application Using Arm GCC