Command-line operations#
SEC also offers a command-line interface, enabling integration in automated environments or customization of image building/burning procedure. Operation requires a verb (command) identifying the top-level operation (building, flashing, provisioning, generating keys or detecting the list of USB devices) and additional operation-specific options.
To display the available commands, arguments, and examples, run the following command from the command prompt:
c:/nxp/SEC_Provi_25.09/bin/securep.exe -h
To display the available arguments for a specific command, run the following command from the command prompt:
c:/nxp/SEC_Provi_25.09/bin/securep.exe <command> -h
Note: The location of the SEC Tool application is subject to the installation folder.
All the supported commands and arguments used in the command line as described in chapters below can also be specified in a separate configuration JSON file. This JSON file is then passed as a command-line argument, see Example how to use args-file arguments.
Table args-file argument
Argument |
Description |
|---|---|
|
Path to the JSON file with CLI arguments allowing to specify all arguments in one file. The path is absolute or relative to the current working directory. The file format is specified by |
Build#
With the build command, you can perform actions that you can otherwise perform in the Build image view of SEC.
The following arguments are available to the build command:
Table Build-specific arguments
Argument |
Description |
|---|---|
|
Show this help message and exit. |
|
Path to JSON with configuration of additional images for the build. The file format is specified by the schema |
|
JSON file with the BEE configuration. See the schema/bee_image_encryption_schema_v2.json in the installation folder. The parameter is applicable for encrypted XIP (BEE user keys) boot type only. |
|
Secure boot type. Run securep –help to see all supported boot types. |
|
Path to JSON file with USER CFPA configuration. It is recommended to export the file from the PFR Configuration dialog. |
|
Path to JSON file with USER CMPA configuration. It is recommended to export the file from the PFR Configuration dialog. |
|
Path to the public CSF key file that is used for signing the image. If not specified then it is derived from the img-cert pathname according to the HAB4 PKI Tree naming convention. |
|
Path to the Device Configuration Data binary file. |
|
32/48/64 HEX characters: data encryption key used for AHAB encryption. The argument is applicable for processors with the AHAB security system. |
|
Target processor. The list of supported processors is displayed using command |
|
JSON file with dual image boot configuration; file format is specified by schema/dual_image_boot_schema_v?.json. The argument is applicable for processors that supports dual image boot |
|
Path to the EdgeLock Enclave (ELE) firmware file. The argument is applicable for encrypted boot types for processors with the AHAB security system. |
|
Version of the application image firmware. |
|
JSON file with the IEE configuration. See the schema/iee_image_encryption_schema_v?.json in the installation folder. The parameter is applicable for IEE encrypted boot type only. |
|
The version of the bootable image can be either in 4-bytes format, for example, 0xFFFE0001 (the lower 2 bytes are the real version number, and the upper 2 bytes are the invert value of lower 2 bytes) or just the real version number (2 bytes). The argument is only applicable for processors that support the image version on the build tab. |
|
Path to the public IMG key file that is used for signing the image. It is recommended to use the command with a workspace with already initialized key management. If the keys are not specified in the workspace settings file, they are imported. |
|
JSON file with PRINCE configuration; file format is specified by schema/prince_config_schema_v?.json |
|
32-bit value: Keyblob encryption key identifier. The argument is applicable for processors with the AHAB security system. |
|
Key source for RT5xx/6xx secured images |
|
Requested life-cycle state of the processor. The list of supported IDs is displayed using command |
|
JSON file with the OTFAD configuration. See the schema/otfad_image_encryption_schema_v?.json in the installation folder. The parameter is applicable for OTFAD encrypted boot type only. |
|
Path to JSON file with USER OTP configuration. It is recommended to export the file from the OTP Configuration dialog. |
|
JSON file with PRINCE configuration. See bin/schema/prince_config_schema_v<version>.json in the SEC installation folder. |
|
Path to JSON file with USER ROMCFG configuration. It is recommended to export the file from the IFR Configuration dialog. |
|
Save workspace settings. |
|
64 HEX characters: Key used as key encryption key to handle SB2 file; Needed only for Secure Binary images; If not specified, it is taken from workspace |
|
Generate build script only, do not launch it |
|
The HAB encryption algorithm, default is processor-specific. |
|
Source image path for building the boot image. |
|
Start address of the executable image data within the source image. Applicable and required only for binary source images. |
|
Target image path for building the boot image. |
|
Trust provisioning type. |
|
Either |
|
Key applicable for RT5xx/6xx secured images: for OTP key-source it represents the master key; for key-store it represents the key used for the signature |
|
Increase output verbosity |
|
Workspace location, path to the workspace directory. Note: Any settings from the workspace are loaded automatically. All command-line parameters can be used to override loaded settings. |
|
JSON file with the XIP Encryption with OTPMK configuration. See the schema/xip_enc_otpmk_schema_v?.json in the installation folder. The argument is applicable for XIP encrypted (BEE OTPMK) and XIP encrypted (OTFAD OTPMK) boot types only. |
|
Path to YAML or binary file with the XMCD configuration (simplified or full); for file format, see the SPSDK command |
Table Boot-device arguments (mutually exclusive)
Argument |
Description |
|---|---|
|
Predefined boot memory. Run |
|
File with boot memory configuration |
|
Boot memory type, one of the following types: |
Write#
With the write command, you can perform actions that you can otherwise perform in the Write image view of SEC.
The following arguments are available to the write command:
Table Write-specific arguments
Argument |
Description |
|---|---|
|
Show this help message and exit |
|
Source image path to be uploaded to the target |
|
JSON file with parameters needed in write and fuses to be burnt by write script (or shadow registers). See the |
|
Requested life-cycle state of the processor. The list of supported IDs is displayed using command |
|
Trust provisioning type. |
|
Increase output verbosity |
|
Target processor. The list of supported processors is displayed using command |
|
Secure boot type. Run |
|
Generate script only, do not launch |
|
Workspace location. Note: Any settings from the workspace are loaded automatically. All command-line parameters can be used to override loaded settings. |
|
Select a debug probe. Use `–debug-probe auto` to select any debug probe. Use `–debug-probe invalid` to list all connected debug probes. |
For boot-device arguments, see Table Boot-device arguments (mutually exclusive)
Table Connection arguments (mutually exclusive)
Argument |
Description |
|---|---|
|
Connect to target over USB HID device denoted by vid/pid. USB HID connection is default. vid/pid can be specified in decimal form (for example, |
|
Connect to target over UART. Specify COM port (see |
|
Connect to target over I2C via USB bridge. Specify I2C device address and clock in kHz. SIO device is autoselected if the |
|
Connect to target over SPI via USB bridge. Specify SPI clock in kHz, polarity (SPI CPOL option) and phase (SPI CPHA option). SIO device is autoselected if the –sio-device argument is not specified. Example: |
|
Connect to target over UART with a specified baud rate. –uart argument has to be specified too. Example: |
|
Connect to target over USB-SIO (I2C or SPI) via a specified SIO device. |
Note: For connection to the board, a USB or Serial port has to be specified. If nothing is specified, USB autodetection is applied.
Generate keys#
With the Generate command, you can perform actions that you can otherwise perform in the Generate Keys view. Compared to GUI, command-line functionality is restricted.
The following arguments are available to the generate command:
Table generate-specific arguments
Argument |
Description |
|---|---|
|
Show this help message and exit |
|
File with the keys configuration |
|
Target processor. The list of supported processors is displayed using command |
|
Secure boot type. Run |
|
Generate script only, do not launch |
|
Workspace location. Note: Any settings from the workspace are loaded automatically. All command-line parameters can be used to override loaded settings. |
For boot-device arguments, see Table Boot-device arguments (mutually exclusive)
Manufacture#
Manufacture command allows running the selected script several times in parallel, each time for a different connection. The following arguments are available to the manufacture command:
Table Manufacture-specific arguments
Argument |
Description |
|---|---|
|
Show this help message and exit |
|
Path to the script to be executed |
|
Parameters of the script. For more information, see |
|
List of all connections devices to be used in manufacturing, in format |
Devices info#
With the devices-info command, you can get information about supported processors and their supported boot devices.
The devices-info command have two modes:
Mode |
Description |
|---|---|
|
Information about supported processors and their supported boot devices. This mode is default. |
|
Information about supported boot devices memory. |
The following arguments are available for the devices-info command:
Argument |
Description |
|---|---|
|
Show this help message and exit. |
|
Device name substring, which is searched in the processor. For boot devices, the whole name of processor is needed to show supported memories. If not provided, unfiltered data are returned. |
|
Format of the output. Default is json for file output, txt for STDOUT. For processors json, see schema/devices_info_schema_v?.json. For boot devices json, see schema/boot_devices_info_schema_v?.json |
|
Path to a file where to store the output. If not provided, the output is printed to STDOUT. |
Test Connection#
The test-connection command performs a processor-specific connection test. The device must be specified either in the workspace or via the command-line option. If no connection is specified in the workspace or as an option, the default connection is used. The connection test is successful if a matching device is connected and is in ISP mode.
Supported arguments
Argument |
Description |
|---|---|
|
Show this help message and exit. |
|
Increase output verbosity |
|
Workspace location. |
|
Target processor. The list of supported processors is displayed using command |
Table Connection arguments (mutually exclusive)
Argument |
Description |
|---|---|
|
Connect to target over USB HID device denoted by vid/pid. USB HID connection is default. vid/pid can be specified in decimal form (for example, |
|
Connect to target over UART. Specify COM port (see |
|
Connect to target over I2C via USB bridge. Specify I2C device address and clock in kHz. SIO device is autoselected if the |
|
Connect to target over SPI via USB bridge. Specify SPI clock in kHz, polarity (SPI CPOL option) and phase (SPI CPHA option). SIO device is autoselected if the –sio-device argument is not specified. Example: |
|
Connect to target over UART with a specified baud rate. –uart argument has to be specified too. Example: |
|
Connect to target over USB-SIO (I2C or SPI) via a specified SIO device. |
Detect USB devices#
The detect command identifies any processor connected via USB. For detection to succeed, the processor must be in ISP mode.
Start flashloader#
Start the flashloader on the RT1xxx processor. The following arguments are available for the start-flashloader command:
Argument |
Description |
|---|---|
|
Show this help message and exit. |
|
Increase output verbosity |
|
Workspace location. |
|
Generate script only, do not launch. |
Table Connection arguments (mutually exclusive)
Argument |
Description |
|---|---|
|
Connect to target over USB HID device denoted by vid/pid. USB HID connection is default. vid/pid can be specified in decimal form (for example, |
|
Connect to target over UART. Specify COM port (see |
|
Connect to target over I2C via USB bridge. Specify I2C device address and clock in kHz. SIO device is autoselected if the |
|
Connect to target over SPI via USB bridge. Specify SPI clock in kHz, polarity (SPI CPOL option) and phase (SPI CPHA option). SIO device is autoselected if the –sio-device argument is not specified. Example: |
|
Connect to target over UART with a specified baud rate. –uart argument has to be specified too. Example: |
|
Connect to target over USB-SIO (I2C or SPI) via a specified SIO device. |
Apply settings#
Command apply-settings supports two main use cases
Modifying an existing workspace
Creating a new workspace
For modifying an existing workspace, specify the path to the workspace and the options to change. General options can be used for this purpose.
For creating a new workspace, at minimum, the boot-device and device options must be specified.
Argument |
Description |
|---|---|
|
Show this help message and exit. |
|
Increase output verbosity |
|
Workspace location. |
|
Requested life-cycle state of the processor. The list of supported IDs is displayed using command |
|
Trust provisioning type. |
|
Target processor. The list of supported processors is displayed using command |
|
Secure boot type. Run |
|
Predefined boot memory. Run |
|
File with boot memory configuration |
|
Boot memory type. Default-predefined boot memory of this type is set. |
Table Connection arguments (mutually exclusive)
Argument |
Description |
|---|---|
|
Connect to target over USB HID device denoted by vid/pid. USB HID connection is default. vid/pid can be specified in decimal form (for example, |
|
Connect to target over UART. Specify COM port (see |
|
Connect to target over I2C via USB bridge. Specify I2C device address and clock in kHz. SIO device is autoselected if the |
|
Connect to target over SPI via USB bridge. Specify SPI clock in kHz, polarity (SPI CPOL option) and phase (SPI CPHA option). SIO device is autoselected if the –sio-device argument is not specified. Example: |
|
Connect to target over UART with a specified baud rate. –uart argument has to be specified too. Example: |
|
Connect to target over USB-SIO (I2C or SPI) via a specified SIO device. |
Environment variables in filepath-based arguments#
SEC Tool accepts environment variables in all arguments specifying paths, for example:
securep.exe -w /workspaces/mcuxprovi --device MIMX9596 --boot-device-type
onchip_ram --boot-type unsigned build --additional-images
additional_images_cfg.json --ele-firmware
"${MCUX_SDK_16}\firmware\edgelock\mx95a0-ahab-container.img" --save-settings
Command-line examples#
Example: How to build and write an image for configuration stored in the workspace folder#
In this example, it is assumed that the GUI was already used to prepare complete configuration within a workspace (keys generated, build image configured, write image configured).
securep.exe -w /workspaces/mcuxprovi build
securep.exe -w /workspaces/mcuxprovi write
For detailed examples, use the following command:
securep.exe print-cli-examples
Example how to use args-file arguments#
In the following examples, CLI arguments are converted to the JSON file.
Arguments in the command line for build:
securep.exe -w /workspaces/mcuxprovi --device MIMX9596 --boot-device-type
onchip_ram --boot-type unsigned build --additional-images
additional_images_cfg.json --ele-firmware mx95a0-ahab-container.img --save-
settings
Usage of args-file argument for above build arguments:
securep.exe --args-file args_file_build.json
args_file_build.json content (only the first additional image is listed):
{
"cli_args": {
"-w": "/workspaces/mcuxprovi",
"--device": "MIMX9596",
"--boot-device-type": "onchip_ram",
"--boot-type": "unsigned",
"build": [],
"--additional-images": {
"images": [
{
"entry_type": "oei_ddr",
"container_set": "#1",
"extra_settings": {
"lpddr_imem_path": "${ENV_VAR_DDR}/lpddr5_imem_v202311.bin",
"lpddr_imem_qb_path": "${ENV_VAR_DDR}/lpddr5_imem_qb_v202311.bin",
"lpddr_dmem_path": "${ENV_VAR_DDR}/lpddr5_dmem_v202311.bin",
"lpddr_dmem_qb_path": "${ENV_VAR_DDR}/lpddr5_dmem_qb_v202311.bin",
"oei_ddr_path": "source_images/oei-m33-ddr.bin"
}
}
]
},
"--ele-firmware": "source_images/mx95a0-ahab-container.img",
"--save-settings": []
}
}
Arguments in command line for write:
securep.exe -w /workspaces/mcuxprovi --device MIMX9596 --boot-device-type
onchip_ram --boot-type unsigned write --source-image bootable_images/flash.bin
Usage of args-file argument for above write arguments:
securep.exe -w /workspaces/mcuxprovi --args-file args_file_write.json
args_file_write.json content:
{
"cli_args": {
"--device": "MIMX9596",
"--boot-device-type": "onchip_ram",
"--boot-type": "unsigned",
"write": [],
"--source-image": "bootable_images/flash.bin"
}
}
Arguments passed directly in the command line are combined together with arguments in the args-file. Arguments cannot be specified in both places.
Command-line tools#
SEC uses the following command-line tools to generate keys and build/write the image:
openssl : Key generation
spsdk : Secure Provisioning SDK, for more information, see main menu > Help > SPSDK Online Documentation. The following tools are available as part of SPSDK:
blhost : Replacement for the legacy blhost tool
dk6prog : Tool for reading and programming flash memory of DK6 target devices.
el2go-host : Managing the EdgeLock 2GO provisioning operations
lpcprog : Utility for communication with the bootloader on LPC8xx target.
nxpcrypto : Operations with keys and certificates
nxpdebugmbox : Debug mailbox and debug credential file generator tool
nxpdevhsm : The application is designed to create an SB3 provisioning file for initial provisioning of the device by the OEM.
nxpdevscan : Utility that detects NXP devices connected to the host PC over USB, UART, I2C, and SPI connections
nxpdice : Application designed to cover DICE-related operations.
nxpele : Utility for communication with the EdgeLock Enclave on target.
nxpfuses : NXP Fuse Tool.
nxpimage : Builds bootable image and SB files
nxpmemcfg : Collection of utilities for memory configuration operations.
nxpshe : NXP tool for working with SHE (Secure Hardware Extension).
nxpuuu : The application for image deployment for i.MX MPUs. It is based on libUUU (universal update utility).
nxpwpc : Utility covering WPC operations.
pfr : Generating protected flash region files (cmpa/cfpa) and IFR.
sdphost : Replacement for the legacy sdphost utility
sdpshost : Utility for communication with ROM on i.MX targets using SDPS protocol (i.MX8/9).
shadowregs : Shadow registers control tool.
imgtool : MCUboot’s image signing and key management