MCUXpresso SDK Documentation

Building the binary file

Building the binary file#

This section describes the required steps for obtaining the binary file for usage with the board. The Connectivity Test Application is available in the package location below:

<sdk_folder_path>\boards\<board_name>\wireless_examples\ieee-802.15.4\connectivity_test\bm\iar

Where <board name> is:

  • k32w148evk for K32W1480-EVK

  • frdmmcxw71 for FRDM-MCXW71

  • frdmmcxw72 for FRDM-MCXW72

  • mcxw71evk for MCX-W71-EVK

  • mcxw72evk for MCX-W72-EVK