MCUXpresso SDK Documentation

Integration and APIs

Contents

Integration and APIs#

Integration#

All the APIs referenced in this section are available in the the full-featured libraries.

  • lib_ble_OPT_host_cm33_iar.a (for IAR projects)

  • lib_ble_OPT_host_cm33_gcc.a (for MCUX projects).

Parent topic:Bluetooth LE Connection Handover Integration and APIs

Connection Handover API availability#

Gap_HandoverGetDataSize#

bleResult_t Gap_HandoverGetDataSize(deviceId_t deviceId, uint32_t *pDataSize);

Description: Returns the size in octets of the Handover Data for the given peer device id.

Parameters:

  • deviceId: Peer device identifier.

  • pDataSize: Pointer to the size in octets of the Handover Data.

Returns: gBleSuccess_c or error.

Gap_HandoverGetData#

bleResult_t Gap_HandoverGetData(deviceId_t deviceId, uint8_t *pData);

Description: Copies the data used by the Handover feature for the given peer device id.

Parameters:

  • deviceId: Peer device identifier.

  • pData: Pointer to memory location where the Handover data is to be copied.

Returns: gBleSuccess_c or error.

Gap_HandoverSetData#

bleResult_t Gap_HandoverSetData(uint8_t *pData);

Description: Sets the data used by the Handover feature.

Parameters:

  • pData: Pointer to memory location where the Handover data is found.

Returns: gBleSuccess_c or error.

Gap_HandoverSetLlPendingData#

bleResult_t Gap_HandoverSetLlPendingData(uint16_t connectionHandle, uint8_t *pTxData);

Description: Sets the LL data pending on the target device to be transmitted after handover connect.

Parameters:

  • connectionHandle: Handover connection identifier.

  • pTxData: Pointer to memory location where the pending data is found.

Returns: gBleSuccess_c or error.

Gap_HandoverFreeData#

bleResult_t Gap_HandoverFreeData(void);

Description: Frees reference to handover data provided through Gap_HandoverSetData().

Returns: gBleSuccess_c or gBleInvalidState_c if handover data reference is not set.

Gap_HandoverGetTime#

bleResult_t Gap_HandoverGetTime(void);

Description: Gets timing information from Link Layer to be used in Handover process.

Returns: gBleSuccess_c or error.

Gap_HandoverSuspendTransmit#

bleResult_t Gap_HandoverSuspendTransmit(deviceId_t deviceId, bleHandoverSuspendTransmitMode_t mode, uint16_t eventCounter, uint8_t noOfConnIntervals);

Description: Suspends TX for the given connection.

Parameters:

  • deviceId: Peer device identifier.

  • mode: Mode.

  • eventCounter: Event counter.

  • noOfConnIntervals: Number of connection intervals during which TX is suspended. Use 0 for manual resume.

Returns: gBleSuccess_c or error.

Gap_HandoverResumeTransmit#

bleResult_t Gap_HandoverResumeTransmit(deviceId_t deviceId);

Description: Resumes TX for the given connection.

Parameters:

  • deviceId: Peer device identifier.

Returns: gBleSuccess_c or error.

Gap_HandoverAnchorNotification#

bleResult_t Gap_HandoverAnchorNotification(deviceId_t deviceId, bleHandoverAnchorNotificationEnable_t enable, uint8_t noOfReports);

Description: Enables or disables anchor notifications for the given peer.

Parameters:

  • deviceId: Peer device identifier.

  • enable: Enables or disables notifications.

  • noOfReports: Number of reports to receive (0 for manual stop).

Returns: gBleSuccess_c or error.

Gap_HandoverAnchorSearchStart#

bleResult_t Gap_HandoverAnchorSearchStart(gapHandoverAnchorSearchStartParams_t *pSearchParams);

Description: Starts anchor search with the given parameters.

Parameters:

  • pSearchParams: Pointer to structure containing anchor search parameters. The structure contains:

    • startTime625: Slot of the anchor point timing of the connection event.

    • startTimeOffset: Slot offset of the anchor point timing of the connection event.

    • lastRxInstant: Last successful access address reception instant (unit 625 us).

    • accessAddress: Access address (4 bytes).

    • crcInit: CRC initialization value (3 bytes).

    • channelMap: Channel map (5 bytes, FF FF FF FF 1F if all channels are used).

    • connInterval: Connection interval (unit 1.25ms).

    • latency: Latency (unit connection interval).

    • supervisionTimeout: Supervision timeout (unit 10ms).

    • eventCounter: Current connection event counter.

    • centralSca: Sleep clock accuracy (0 to 7).

    • role: Role (0 for central and 1 for peripheral).

    • centralPhy: TX/RX PHY.

    • seqNum: Sequence number; bits 1-0: latest received SN and NESN; bits 5-4: latest transmitted SN and NESN.

    • hopAlgo2: Hop algorithm (0/1 for hop algorithm #1 or #2).

    • unmappedChannelIndex: Unmapped channel index (used only for hop algorithm #1).

    • hopIncrement: Hop increment.

    • ucNbReports: Number of connection intervals to monitor (0: continuous, 1-255: automatic stop).

    • uiEventCounterAdvance: Event counter delay to perform the search (0 to start ASAP).

    • timeout: Timeout in connection intervals (0 if no timeout).

    • timingDiffSlot: Slot difference of the LL timing.

    • timingDiffOffset: Slot offset difference of the LL timing.

    • mode: Search mode setting.

    • reportLatency: gHandoverAnchorMonitorEvent_c report latency. Applies only after a valid RSSI detection (0 = send all HCI events, use gHandoverAnchorMonitorReportLatencySendAll_c; 1-254 = skip that many events with valid RSSI; 255 = drop all HCI events with valid RSSI, use gHandoverAnchorMonitorReportLatencyDropAll_c).

    • connEvtRxLatency: Connection events RX operation latency. Applies only after a valid RSSI detection (0 = monitor all connection events for the radio RX; 1-255 = skip that many connection events during the radio RX).

Returns: gBleSuccess_c or error.

Gap_HandoverAnchorSearchStop#

bleResult_t Gap_HandoverAnchorSearchStop(uint16_t connHandle);

Description: Stops anchor search for the given connection handle.

Parameters:

  • connHandle: Connection handle for which to stop the anchor search.

Returns: gBleSuccess_c or error.

Gap_HandoverTimeSyncTransmit#

bleResult_t Gap_HandoverTimeSyncTransmit(gapHandoverTimeSyncTransmitParams_t *pTransmitParams);

Description: Starts time sync advertising with given parameters.

Parameters:

  • pTransmitParams: Pointer to structure containing time sync transmit parameters. The structure contains:

    • enable: Enables or disables the transmit operation (0 = disable, 1 = enable).

    • advChannel: BLE channel to use for advertising (0 to 39).

    • deviceAddress: Packet identifier, can be the BD address or any value (6 bytes).

    • phys: PHY setting (0 = 1M, 1 = 2M, 2 = LR S8, 3 = LR S2).

    • txPowerLevel: TX Power level (0 to 31).

    • txIntervalSlots625: Packet interval in slots (4 to 255).

Returns: gBleSuccess_c or error.

Gap_HandoverTimeSyncReceive#

bleResult_t Gap_HandoverTimeSyncReceive(gapHandoverTimeSyncReceiveParams_t *pReceiveParams);

Description: Starts time sync scanning with the given parameters.

Parameters:

  • pReceiveParams: Pointer to structure containing time sync receive parameters. The structure contains:

    • enable: Enables or disables the receive operation (0 = disable, 1 = enable).

    • scanChannel: BLE channel to use for scanning (0 to 39).

    • deviceAddress: Packet identifier, can be the BD address or any value (6 bytes).

    • phys: PHY setting (0 = 1M, 1 = 2M, 2 = LR S8, 3 = LR S2).

    • stopWhenFound: One-shot setting (0 = continue scanning, 1 = stop when packet is found).

Returns: gBleSuccess_c or error.

Gap_HandoverGetConnParams#

bleResult_t Gap_HandoverGetConnParams(uint16_t connHandle, gapConnectionCallback_t connectionCallback, uint8_t anchorNotification);

Description: Connects to a peer device initialized through the Connection Handover procedure.

Parameters:

  • connHandle: Handover Connection handle.

  • connectionCallback: Pointer to the connection event handler function.

  • anchorNotification: Anchor search setting after handover, 0 - stop anchor notification, 1 - keep anchor notification.

Returns: gBleSuccess_c or error.

Gap_HandoverDisconnect#

bleResult_t Gap_HandoverDisconnect(deviceId_t deviceId);

Description: Disconnects a peer device for which the connection was handed over to another device.

Parameters:

  • deviceId: Peer device identifier.

Returns: gBleSuccess_c or error.

Gap_HandoverInit#

bleResult_t Gap_HandoverInit(void);

Description: Initializes the connection handover feature. Must be called before Ble_Initialize().

Returns: gBleInvalidState_c if Ble_Initialize() was already called, gBleSuccess_c otherwise.

Gap_HandoverSetSkd#

bleResult_t Gap_HandoverSetSkd(uint8_t nvmIndex, uint8_t *pSkd);

Description: Sets the SKD of the connection that is to be handed over. Used only if gAppSecureMode_d is enabled in the application. Requires Handover Data to be set.

Parameters:

  • nvmIndex: Bonding Data NVM index.

  • pSkd: Pointer to 16 octets SKD.

Returns: gBleInvalidState_c if Ble_Initialize() was already called, gBleSuccess_c otherwise.

Gap_HandoverGetCsLlContext#

bleResult_t Gap_HandoverGetCsLlContext(deviceId_t deviceId);

Description: Copies the LL CS-related context data for the given peer device id.

Parameters:

  • deviceId: Peer device identifier.

Returns: gBleSuccess_c or error.

Gap_HandoverSetCsLlContext#

bleResult_t Gap_HandoverSetCsLlContext(deviceId_t deviceId, uint16_t mask, uint8_t contextLength, uint8_t *pContextData);

Description: Sets the CS-related context data into the LL, for the given peer device id.

Parameters:

  • deviceId: Peer device identifier.

  • mask: Context data bitmask (used by the LL).

  • contextLength: Length of the context data.

  • pContextData: Pointer to context data.

Returns: gBleSuccess_c or error.

Gap_HandoverUpdateConnParams#

bleResult_t Gap_HandoverUpdateConnParams(gapHandoverUpdateConnParams_t *pConnParams);

Description: Updates the channel map and/or PHY used in the current anchor monitoring process.

Parameters:

  • pConnParams: Pointer to connection parameters to be updated.

Returns: gBleSuccess_c or error.

Gap_HandoverApplyConnectionUpdateProcedure#

bleResult_t Gap_HandoverApplyConnectionUpdateProcedure(gapHandoverApplyConnectionUpdateProcedure_t *pConnParams);

Description: Applies the new connection parameters in case of Connection Update Procedure on the active controller.

Parameters:

  • pConnParams: Pointer to connection parameters to be applied.

Returns: gBleSuccess_c or error.

Connection Handover Events#

The following events can be received through the GAP generic callback during the handover operations:

gHandoverGetComplete_c (0x31)#

Description: Event generated when handover data get operation is complete.

Event Data: handoverGetData_t containing:

  • status: Command status.

  • pData: Pointer to connection handover data.

gHandoverSetComplete_c (0x32)#

Description: Event generated when handover data set operation is complete.

Event Data: handoverSetData_t containing:

  • status: Command status.

  • pData: Pointer to connection handover data.

gHandoverGetCsLlContextComplete_c (0x33)#

Description: Event generated when handover CS LL context data get operation is complete.

Event Data: handoverGetCsLlContext_t containing:

  • status: Command status.

  • responseMask: LL context bitmap indicating the Channel Sounding context.

  • llContextLength: Context data length.

  • llContext: LL Context data.

gHandoverSetCsLlContextComplete_c (0x34)#

Description: Event generated when handover CS LL context data set operation is complete.

Event Data: Status of the operation.

gHandoverGetTime_c (0x35)#

Description: Event generated when Handover Get Time command is complete.

Event Data: handoverGetTime_t containing:

  • status: Command status.

  • slot: LL timing slot counter (unit 625us).

  • us_offset: LL timing slot offset (0 to 624, unit us).

gHandoverSuspendTransmitComplete_c (0x36)#

Description: Event generated when Handover Suspend Transmit command is complete.

Event Data: handoverSuspendTransmitCompleteEvent_t containing:

  • connectionHandle: Connection identifier.

  • noOfPendingAclPackets: Number of pending ACL packets.

  • sizeOfPendingAclPackets: Pending ACL packet data size.

  • sizeOfDataTxInOldestPacket: Size of data transmitted and acked in the oldest ACL packet.

  • sizeOfDataNAckInOldestPacket: Size of data transmitted but not acked in the oldest ACL packet.

gHandoverResumeTransmitComplete_c (0x37)#

Description: Event generated when Handover Resume Transmit command is complete.

Event Data: handoverResumeTransmitCompleteEvent_t containing:

  • connectionHandle: Connection identifier.

gHandoverAnchorNotificationStateChanged_c (0x38)#

Description: Event generated when Handover Anchor Notification command is complete.

Event Data: handoverAnchorNotificationStateChanged_t containing:

  • connectionHandle: Connection identifier.

gHandoverAnchorSearchStarted_c (0x39)#

Description: Event generated when Handover Anchor Search Start command is complete.

Event Data: handoverAnchorSearchStart_t containing:

  • status: Command status.

  • connectionHandle: Connection identifier.

gHandoverAnchorSearchStopped_c (0x3A)#

Description: Event generated when Handover Anchor Search Stop command is complete.

Event Data: handoverAnchorSearchStop_t containing:

  • status: Command status.

  • connectionHandle: Connection identifier.

gHandoverTimeSyncTransmitStateChanged_c (0x3B)#

Description: Event generated when Handover Time Sync Transmit command is complete.

Event Data: Status of the operation.

gHandoverTimeSyncReceiveComplete_c (0x3C)#

Description: Event generated when Handover Time Sync Receive command is complete.

Event Data: Status of the operation.

gHandoverAnchorMonitorEvent_c (0x3D)#

Description: Event received from Controller - Handover Anchor Monitor.

Event Data: handoverAnchorMonitorEvent_t containing:

  • connectionHandle: Connection identifier.

  • connEvent: Current connection event counter.

  • rssiRemote: RSSI of the packet from the remote device (+127 if not available).

  • lqiRemote: LQI (Link Quality Indicator) of the packet from the remote device.

  • statusRemote: Status of the packet from the remote device.

  • rssiActive: RSSI of the packet from the active device (+127 if not available).

  • lqiActive: LQI (Link Quality Indicator) of the packet from the active device.

  • statusActive: Status of the packet from the active device.

  • anchorClock625Us: Slot of the anchor point timing of the connection event.

  • anchorDelay: Slot offset of the anchor point timing of the connection event.

  • chIdx: BLE channel index.

  • ucNbReports: Number of remaining reports to receive.

gHandoverTimeSyncEvent_c (0x3E)#

Description: Event received from Controller - Handover Time Sync.

Event Data: handoverTimeSyncEvent_t containing:

  • txClkSlot: Transmitter packet start time in slot (625 us).

  • txUs: Transmitter packet start time offset inside the slot (0 to 624 us).

  • rxClkSlot: Receiver packet start time in slot (625 us).

  • rxUs: Receiver packet start time offset inside the slot (0 to 624 us).

  • rssi: RSSI value.

gHandoverConnParamUpdateEvent_c (0x3F)#

Description: Event received from Controller - Handover Connection Parameters Update.

Event Data: handoverConnParamUpdateEvent_t containing:

  • status: Status indicating the event trigger source.

  • connectionHandle: Connection identifier.

  • ulTxAccCode: Access address.

  • aCrcInitVal: CRC initialization value (3 bytes).

  • uiConnInterval: Connection interval (unit 1.25ms).

  • uiSuperTO: Supervision timeout (unit 10ms).

  • uiConnLatency: Latency (unit connection interval).

  • aChMapBm: Channel map (5 bytes).

  • ucChannelSelection: Hop algorithm (0/1 for algorithm #1 or #2).

  • ucHop: Hop increment.

  • ucUnMapChIdx: Unmapped channel index.

  • ucCentralSca: Sleep clock accuracy.

  • ucRole: Role (0 for central and 1 for peripheral).

  • aucRemoteMasRxPHY: TX/RX PHY.

  • seqNum: Sequence number.

  • uiConnEvent: Current connection event counter.

  • ulAnchorClk: Slot of the anchor point timing.

  • uiAnchorDelay: Slot offset of the anchor point timing.

  • ulRxInstant: Last successful access address reception instant.

gHandoverFreeComplete_c (0x46)#

Description: Event generated when handover data free operation is complete.

Event Data: Status of the operation.

gHandoverUpdateConnParamsComplete_c (0x47)#

Description: Event generated when Handover Update Connection Parameters command is complete.

Event Data: handoverUpdateConnParams_t containing:

  • status: Command status.

  • connectionHandle: Connection identifier.

gHandoverLlPendingData_c (0x4A)#

Description: Event indicating ACL Data pending to be transmitted by the LL.

Event Data: handoverLlPendingDataIndication_t containing:

  • dataSize: Pending HCI ACL data packet size.

  • pData: Pointer to message containing the HCI ACL data packet (should be freed by the application).

gHandoverAnchorMonitorPacketEvent_c (0x44)#

Description: Event received from Controller - Handover Anchor Monitor Packet.

Event Data: handoverAnchorMonitorPacketEvent_t containing:

  • packetCounter: Packet counter, incremented for each event.

  • connectionHandle: Connection identifier.

  • statusPacket: Status of the packet.

    • b0: CRC status - valid (1) or invalid (0).

    • b1: packet transmitter - central (1) or peripheral (0).

  • phy: PHY (0/1/2/3 for 1M/2M/LR S8/LR S2).

  • chIdx: BLE channel index.

  • rssiPacket: RSSI of the packet (+127 if not available).

  • lqiPacket: LQI (Link Quality Indicator) of the packet.

  • connEvent: Current connection event counter.

  • anchorClock625Us: Slot value of packet start time (in 625us unit).

  • anchorDelay: Slot offset value of packet start time (in 1us unit).

  • ucNbConnIntervals: Number of remaining connection intervals to monitor.

  • pduSize: PDU length.

  • pPdu: Pointer to PDU data (must be freed by the application).

gHandoverAnchorMonitorPacketContinueEvent_c (0x45)#

Description: Event received from Controller - Handover Anchor Monitor Packet Continue.

Event Data: handoverAnchorMonitorPacketContinueEvent_t containing:

  • packetCounter: Packet counter, incremented for each event.

  • connectionHandle: Connection identifier.

  • pduSize: PDU length.

  • pPdu: Pointer to PDU data (must be freed by the application).

gHandoverConnectionUpdateProcedureEvent_c (0x4F)#

Description: Event reporting new connection parameters indicated during the Connection Update procedure.

Event Data: handoverConnectionUpdateProcedureEvent_t containing:

  • connectionHandle: Connection identifier.

  • winSize: Transmit window size value (in 1.25 ms units).

  • winOffset: Transmit window offset value (in 1.25 ms units).

  • interval: Connection interval value (in 1.25 ms units).

  • latency: Connection peripheral latency value.

  • timeout: Connection supervision timeout value (in 10 ms units).

  • instant: Connection event counter value when new parameters will be applied.

  • currentEventCounter: Current connection event counter.

gHandoverApplyConnectionUpdateProcedureComplete_c (0x50)#

Description: Event reporting completion of the Connection Update procedure application.

Event Data: handoverApplyConnectionUpdateProcedure_t containing:

  • connectionHandle: Connection identifier.