MCUXpresso SDK Documentation

Bug fixes and/or feature enhancements#

Firmware version: 18.99.2.p7.19#

Component

Description

-

NA

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.2.p7.19 to 18.99.2.p49.9#

Component

Description

-

NA

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.2.p49.9 to 18.99.2.p155#

Component

Description

Bluetooth

  • Audio lost occurs due to periodic adv sync lost, during 2 BIS 44.1kHz unencrypted streams with 1M PHY configuration.
  • BIS sync loss may occur in long audio streaming sessions.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.2.p155 to 18.99.2.p66.30#

Component

Description

Wi-Fi

  • 802.11R Fast BSS roaming works only with hostapd and does not work with standard APs (supporting 11R)

Bluetooth

  • DUT is not able to sustain a connection with the remote device that does extended advertisement with coded PHY configuration.
  • When 2 CIS streams are active, after the first device disconnects followed by the second device disconnecting, the second peripheral device hangs.
  • Audio Play/Pause does not work in BIS case.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.2.p66.30 to 18.99.3.p10.5#

Component

Description

Wi-Fi

  • STAUT not sending Neighbor Advertisement packet after receiving Neighbor Solicitation packet from Ex-AP.
  • Antenna selection time exceeds configured evaluation time

Bluetooth

  • When DUT works as CIS source and CIS Offset is 612us, high packet drops observed which affects the audio streaming.
  • For BIS Source Use Cases, Periodic Interval and ISO Interval should be multiple of each other value.
  • In 1-CIS and 2-CIS, Continuous Audio Glitches are observed with 96 kbps bit rate.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.3.p10.5 to 18.99.3.p17.9#

Component

Description

Wi-Fi

  • After performing independent reset (out-of-band mode), the STAUT fails to connect to the external AP via wlan-connect command, observed command timeout 0x107 error.

Bluetooth

  • Audio glitches observed with Google Pixel 7 Pro streaming audio after CIS is established with DUT.
  • During Call Gateway (CG) / Call Terminal (CT) Use Case, the firmware periodically sends NULL PDU, which results in frequent Audio Glitch on both CG and CT sides.
  • Heavy audio glitches observed with CIS SRC Google Pixel 7 Pro
  • Continuous audio glitches observed in 1 CIS and 2 CIS for 48_3 and 48_4 config.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.3.p17.9 to 18.99.3.p21.154#

Component

Description

Wi-Fi

  • STAUT fail to ping AP backend machine when connected with DFS channel and DUTSTA went in bad state.

Bluetooth

  • CIS Sink frequently fails to acknowledge CIS Source TX PDU.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.3.p21.154 to 18.99.3.p23.16#

Component

Description

-

NA

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.3.p23.16 to 18.99.3.p25.11#

Component

Description

Bluetooth

Packet lost observed in CIS case, which causes audio noise.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.3.p25.11 to 18.99.3.p26.10#

Component

Description

Wi-Fi

During legacy roaming when the “Link Lost” observed the DUTSTA fails to roam

Wi-Fi

During the automated testing of the channel performance, a system hang can occur, with the error message “.sdio_drv_write failed”.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.3.p26.10 to 18.99.3.p27.1#

Component

Description

Wi-Fi

Enabled mbedtls 3.x

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.3.p27.10 to 18.99.8.p10#

Component

Description

Wi-Fi

  • Fail to set band to 2.4G in wifi_test_mode application
  • Enabled mbedtls 3.x

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.8.p10 to 18.99.8.p68#

Component

Description

Wi-Fi

  • Duplicate Packet Reception in JP Region due to Missing BA/ACK Transmission
  • Fixed STA setting wrong primary channel when external AP has incorrect secondary channel offset field.
  • Fixed WPA3 STA datapath ping stuck until next reassociation; fixed DUT TX throughput dropping to 0 or getting stuck in pre-sleep state under stress.
  • Fixed scan results taking more than 5 seconds to appear in AP+STA mode.
  • Fixed RSSI_INFO (0xa4) command timeout when DUT is left idle for extended periods in AP+STA mode.

Bluetooth

  • Sequential Removal of CIS Handles as per current Controller implementation i.e CIS Disconnection sequence should be in sequence => CIS - 4,3,2,1
  • While 4-CIS streaming,audio glitches observed on all CIS SINK with Samsung Galaxy buds
  • Fixed missing Disconnect Complete event from controller causing host to get stuck after ACL link disconnection.
  • Added mechanism to detect BT slave link FST on odd-numbered offset
  • Fixed firmware crash observed after eSCO connection complete event.
  • Fixed BTC ACL link disconnection due to CCM counter not being incremented during encryption
  • Fixed BLE and BTC power backoff not working when BTU power control is disabled in MFG firmware.

Parent topic: Bug fixes and/or feature enhancements

Firmware version: 18.99.8.p68 to 18.99.8.p141#

Component

Description

Wi-Fi

  • The device connects successfully but fails to roam when signal degrades.
  • Fixed an issue where DHCP renewal was not triggered when roaming between independent APs sharing the same SSID
  • Fixed an issue where ping responses failed on the first uAP BSS start in 2.4 GHz
  • Fixed an issue where the DUT failed to fall back to legacy roaming after 802.11k/11v roaming returned no usable target AP

Bluetooth

  • Fixed an issue where the BR/EDR Coex shell app incorrectly initialized the Nighthawk (IW610) module and downloaded firmware instead of IW612, causing NB UART firmware download to fail with “HDR SIG not found” (-22) and subsequently WLAN initialization to fail.
  • Fixed a sporadic LE RX degradation issue , where GATT indication delays exceeding 500 ms were observed due to excessive retransmissions in a concurrent BTC ACL + eSCO + BLE scatternet scenario.
  • Fixed a issue where DUT sends HCI Hardware Error (0x22)
  • Fixed a issue where DUT establishes LE connections with two devices using same connection handle
  • Fixed a issue where Controller will choose connection interval that won’t collide with eSCO link paremeters.

Parent topic: Bug fixes and/or feature enhancements

Parent topic: IW611/IW612 release notes