ZPS_tsAplZdpMgmtDirectJoinReq
This structure is used by the function ZPS_eAplZdpMgmtDirectJoinRequest(). It requests a remote node to allow a particular device to join it (and therefore the network).
The ZPS_tsAplZdpMgmtDirectJoinReqstructure is detailed below.
typedef struct { uint64 u64DeviceAddress; uint8 u8Capability; } ZPS_tsAplZdpMgmtDirectJoinReq;
where:
u64DeviceAddressis the IEEE address of the device to be allowed to joinu8Capabilityis a bitmask of the operating capabilities of the device to be allowed to join. This bitmap is detailed in Table in section ZPS_tsAfNwkJoinIndEvent.
Parent topic:ZDP Request structures