Linux OS host
The following sections provide steps to run a demo compiled with Arm GCC on Linux host.
Set up toolchain
This section contains the steps to install the necessary components required to build and run a MCUXpresso SDK demo application with the Arm GCC toolchain, as supported by the MCUXpresso SDK.
Install GCC Arm embedded tool chain
Download and run the installer from launchpad.net/gcc-arm-embedded. This is the actual toolset (in other words, compiler, linker, and so on). The GCC toolchain should correspond to the latest supported version, as described in the MCUXpresso SDK Release Notes (document MCUXSDKRN).
Note: See Host setup for Linux OS before compiling the application.
Parent topic:Set up toolchain
Add a new system environment variable for ARMGCC_DIR
Create a new system environment variable and name it ARMGCC_DIR. The value of this variable should point to the Arm GCC Embedded tool chain installation path. For this example, the path is:
$ export ARMGCC_DIR=/work/platforms/tmp/gcc-arm-none-eabi-7-2017-q4-major
$ export PATH= $PATH:/work/platforms/tmp/gcc-arm-none-eabi-7-2017-q4-major/bin
Parent topic:Set up toolchain
Parent topic:Linux OS host
Build an example application
To build an example application, follow these steps.
Change the directory to the example application project directory, which has a path similar to the following:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgccFor this example, the exact path is:
<install_dir>/boards/evkmimx8mq/demo_apps/hello_world/armgccRun the
build_debug.shscript on the command line to perform the build. The output is shown as below:$ ./build_debug.sh -- TOOLCHAIN_DIR: /work/platforms/tmp/gcc-arm-none-eabi-7-2017-q4-major -- BUILD_TYPE: debug -- TOOLCHAIN_DIR: /work/platforms/tmp/gcc-arm-none-eabi-7-2017-q4-major -- BUILD_TYPE: debug -- The ASM compiler identification is GNU -- Found assembler: /work/platforms/tmp/gcc-arm-none-eabi-7-2017-q4-major/bin/arm-none-eabi-gcc -- Configuring done -- Generating done -- Build files have been written to: /work/platforms/tmp/nxp/SDK\_2.3.0\_EVK-MIMX8MQ/boards/evkmimx8mq/demo\_apps/hello\_world/armgcc Scanning dependencies of target hello_world.elf \[ 6%\] Building C object CMakeFiles/hello\_world.elf.dir/work/platforms/tmp/nxp/SDK\_2.3.0\_EVK-MIMX8MQ/boards/evkmimx8mq/demo\_apps/hello\_world/hello\_world.c.obj < -- skipping lines -- > [100%] Linking C executable debug/hello_world.elf [100%] Built target hello_world.elf
Parent topic:Linux OS host
Run an example application
This section describes steps to run a demo application using J-Link GDB Server application.
After the J-Link interface is configured and connected, follow these steps to download and run the demo applications:
Connect the development platform to your PC via USB cable between the USB-UART connector and the PC USB connector. If using a standalone J-Link debug pod, also connect it to the SWD/JTAG connector of the board.
Open the terminal application on the PC, such as PuTTY or TeraTerm, and connect to the debug serial port number (to determine the COM port number, see How to determine COM port). Configure the terminal with these settings:
115200 baud rate, depending on your board (reference
BOARD_DEBUG_UART_BAUDRATEvariable in theboard.hfile)No parity
8 data bits
1 stop bit
|

|
Open the J-Link GDB Server application. Assuming the J-Link software is installed, the application can be launched from a new terminal for the MIMX8MQ6_M4 device:
$ JLinkGDBServer -if JTAG -device MIMX8MQ6\_M4 SEGGER J-Link GDB Server V6.22a Command Line Version JLinkARM.dll V6.22g \(DLL compiled Jan 17 2018 16:40:32\) Command line: -if JTAG -device MIMX8MQ6\_M4 -----GDB Server start settings----- GDBInit file: none GDB Server Listening port: 2331 SWO raw output listening port: 2332 Terminal I/O port: 2333 Accept remote connection: yes < -- Skipping lines -- > Target connection timeout: 0 ms ------J-Link related settings------ J-Link Host interface: USB J-Link script: none J-Link settings file: none ------Target related settings------ Target device: MIMX8MQ6\_M4 Target interface: JTAG Target interface speed: 1000 kHz Target endian: little Connecting to J-Link... J-Link is connected. Firmware: J-Link V10 compiled Jan 11 2018 10:41:05 Hardware: V10.10 S/N: 600101610 Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB Checking target voltage... Target voltage: 3.39 V Listening on TCP/IP port 2331 Connecting to target... J-Link found 1 JTAG device, Total IRLen = 4 JTAG ID: 0x5BA00477 \(Cortex-M4\) Connected to target Waiting for GDB connection...
Change to the directory that contains the example application output. The output can be found in using one of these paths, depending on the build target selected:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc/debug<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc/releaseFor this example, the path is:
*<install\_dir\>/boards/evkmimx8mq/demo\_apps/hello\_world/armgcc/debug*Start the GDB client:
$ arm-none-eabi-gdb hello_world.elf GNU gdb (GNU Tools for Arm Embedded Processors 7-2017-q4-major) 8.0.50.20171128-git Copyright (C) 2017 Free Software Foundation, Inc. License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html> This is free software: you are free to change and redistribute it. There is NO WARRANTY, to the extent permitted by law. Type "show copying" and "show warranty" for details. This GDB was configured as "--host=x86_64-linux-gnu --target=arm-none-eabi". Type "show configuration" for configuration details. For bug reporting instructions, please see: <http://www.gnu.org/software/gdb/bugs/>. Find the GDB manual and other documentation resources online at: <http://www.gnu.org/software/gdb/documentation/>. For help, type "help". Type "apropos word" to search for commands related to "word"... Reading symbols from hello_world.elf... (gdb)
Connect to the GDB server and load the binary by running the following commands:
target remote localhost:2331monitor resetmonitor haltload
(gdb) target remote localhost:2331 Remote debugging using localhost:2331 0x1ffe0008 in \_\_isr\_vector \(\) (gdb) monitor reset Resetting target (gdb) monitor halt (gdb) load Loading section .interrupts, size 0x240 lma 0x1ffe0000 Loading section .text, size 0x3858 lma 0x1ffe0240 Loading section .ARM, size 0x8 lma 0x1ffe3a98 Loading section .init\_array, size 0x4 lma 0x1ffe3aa0 Loading section .fini\_array, size 0x4 lma 0x1ffe3aa4 Loading section .data, size 0x64 lma 0x1ffe3aa8 Start address 0x1ffe02f4, load size 15116 Transfer rate: 81 KB/sec, 2519 bytes/write. \(gdb\)
The application is now downloaded and halted at the reset vector. Execute the monitor go command to start the demo application.
(gdb) monitor go
The hello_world application is now running and a banner is displayed on the terminal. If this is not true, check your terminal settings and connections.
|
|
Parent topic:Linux OS host
Parent topic:Run a demo using Arm GCC