Run a TrustZone example application {#GUID-5A9FC9CB-C285-46F0-8DDF-830DBD1877BA}
When running a TrustZone application, the same prerequisites for J-Link/J-Link OpenSDA firmware, and the serial console as for the single core application, apply, as described in Section 6.3, “Run an example application”.
To download and run the TrustZone application, perform steps 1 to 10, as described in Section 5.3, “Run an example application”. These steps are common for both single core and TrustZone applications in Arm GCC.
Then, run these commands:
arm-none-eabi-gdb.exetarget remote localhost:2331monitor resetmonitor haltmonitor exec SetFlashDLNoRMWThreshold = 0x20000load <install\_dir\>/boards/lpcxpresso55s69/trustzone\_examples/hello\_world/cm33\_core0/hello\_world\_ns/armgcc/debug/hello\_world\_ns.elfload <install\_dir\>/boards/lpcxpresso55s69/trustzone\_examples/hello\_world/cm33\_core0/hello\_world\_s/armgcc/debug/hello\_world\_s.elf
The application is now downloaded and halted at the watchpoint. Execute the monitor go command to start the demo application.
|
|
|
|
Parent topic:Run a demo using Arm GCC