MCUXpresso SDK Documentation

sgi_hash

sgi_hash#

Overview#

The SGI PKC application provides examples which demonstrate usage of most available algorithms and a crypto library lightweight testing:

  • AES-128 encryption/decryption, modes ECB/CBC/CTR/GCM/CMAC

  • SHA2-224/256/384/512 (including sha-direct mode)

  • ECC Sign/Verify/Keygen/Keyexchange

Supported Boards#

FRDM-MCXA266
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA266 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END

FRDM-MCXA366
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA366 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END

FRDM-MCXL255
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXL255 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END

FRDM-MCXA577
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA577 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END

FRDM-KW43
Hardware requirements
  • Type-C USB cable

  • FRDM-KW43 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END

FRDM-MCXA287
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXA287 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END

KW43-LOC
Hardware requirements
  • Type-C USB cable

  • KW43-LOC board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END

MCXW70-LOC
Hardware requirements
  • Type-C USB cable

  • MCXW70-LOC board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.


SGI hash example

============================
SHA224 one shot:pass
SHA256 one shot:pass
SHA256 streaming example:pass
SHA256 long message example:pass
SHA384 one shot:pass
SHA512 one shot:pass

============================
RESULT: All 6 test PASS!!
SGI example END