MCXN - OTA update by using SB3 file#
In this walkthrough, the device lifecycle is not changed where possible (for development purposes), so that the device can be restored to its initial state. In real-world scenarios, transitioning the chip to the appropriate lifecycle depends on the specific requirements.
Common information related to SB3 is available in the documentation ‘OTA update by using SB3 file’.
1. Provision the device#
The device must be provisioned to support SB3 processing. To simplify the workflow, the MCUXpresso Secure Provisioning Tool (SEC tool) is used.
To provision the device perform the following steps:
Erase the device
Build the
mcuboot_opensource+ota_mcuboot_basicor theota_rom_basicproject, depending on what you want to evaluateGet the device into ISP mode - on development boards this is typically done by holding the ISP button and pressing the reset button
Open the SEC tool, create a new workspace for the MCXN target device, and test the ISP connection
Switch to PKI management tab
Click Generate keys (leave default settings)

Build Image tab
Boot: Plain signed from IFR/Onchip flash based on
mcuboot_opensourceorota_rom_basiclocationLifecycle: Develop
Select an authentication key and generate CUST_MK_SK and OEM SB seed
Enable Dual image support if you evaluate
ota_rom_basicDefine Image version 1
Target dual boot image: Image 1
Image 1 size:
For MCXN9xx/5xx select 0x100000 (1MB)
For MCXN2xx select 0x80000 (512kB)
Following image is for MCUboot use case

Following image is for ROM only use case

Click Build image
Write image tab
Click Write image

2. Prepare OTA images#
2.1 ROM bootloader only use case#
MCXN uses flash remapping based on the swap mechanism, so the SB3 OTA file always targets the Image 1 memory region.
Build Image tab
Increase the image version from 1 to 2
Build image
Rename the generated SB3 file
bootable_images/ota_rom_basic.sbtoota_rom_basic_image_1_v2.sb
2.2 MCUboot bootloader use case#
Build
ota_mcuboot_basicand sign the image withimgtoolas usual, following the steps in theexample_board_readme.mdfor your board. Copy the signed binary to your$sec_tool_workspace/source_images.Look into the
ota_examples/_common/sb3_templatesdirectory and copy the SB3 configuration templates for your device to your$sec_tool_workspace/configs.MCXN:
mcxn_sb3_cfg_primary_slot.yaml
In the SEC tool, open Tools/SB Editor and click Import to import
sb3_config_mcxn_secondary_slot.yaml.Check and, if necessary, fix the paths to the keys and the image binary.
Click Generate.


Note: Optionally, an initial SB3 file containing the initial (first) ota_mcuboot_basic application for the primary/secondary slot (generated with the additional --pad --confirm imgtool arguments) can be created to simulate the manufacturing process. Otherwise, the initial signed image can also be loaded directly using ISP or another preferred method, as usual.
3. Firmware update#
For demonstration purposes we use the ExtraPutty tool, as this fork of the classic PuTTY has XMODEM support. Alternatively, TeraTerm can be used.
3.1 ROM bootloader only use case#
Run the initial
ota_rom_basicapplication loaded in chapter 1.Note: alternatively, run the unsigned application via a debug session using your preferred IDE (IAR, MCUX, VS Code) - in this case the
imagecommand returns invalid information, as there is no valid image header to parse.
Check the image state and the active flag location with the
imagecommand.Use the active flag location to determine the inactive image slot.
Send the OTA image.
Run the
xmodem_sb3command.Send
ota_rom_basic_image_1_v2.sb, targeting the inactive slot, via Files Transfer/Xmodem (1k).
Reboot the device with
rebootcommandCheck image update with
imagecommand
Here is an example of serial output:
*************************************
* Basic ROM application example *
*************************************
$ image
Flash REMAP_SWAP disabled
IMAGE 0:
<IMG_VERSION 0x1 LENGTH 36820 EXEC_ADDR 0x28004000>
*ACTIVE*
IMAGE 1: Invalid image header
$ xmodem_sb3
Started xmodem processing SB3
Initiated XMODEM-CRC transfer. Receiving... (Press 'x' to cancel)
CCCC
Received 37880 bytes
SB3 has been processed
$
$ reboot
System reset!
*************************************
* Basic ROM application example *
*************************************
$ image
Flash REMAP_SWAP active
IMAGE 0:
<IMG_VERSION 0x1 LENGTH 36820 EXEC_ADDR 0x28004000>
IMAGE 1:
<IMG_VERSION 0x2 LENGTH 36820 EXEC_ADDR 0x28004000>
*ACTIVE*
$
3.2 MCUboot bootloader use case#
Load and run the initial
ota_mcuboot_basicapplication as usual - alternatively, load the initial SB3 viablhostand thereceive-sb-filecommand.Check the image state and the active flag location with the
imagecommand.Use the active flag location to determine the inactive image slot.
Erase the inactive slot with the
image erasecommand.Note: not needed if the SB file contains the erase command.
Send the OTA image.
Run the
xmodem_sb3command.Send
ota_mcuboot_secondary_slot.sb, targeting the inactive slot, via Files Transfer/Xmodem (1k).
Mark the installed image ready for test.
Run the
image testcommand.
Reboot the device with the
rebootcommand.Check the image update with the
imagecommand.Mark the updated slot with the confirm flag using
image accept, and check the state again with theimagecommand.
hello sbl.
Bootloader Version 2.2.0
Primary slot: version=1.0.0+1000
Image 0 Secondary slot: Image not found
Image 0 loaded from the primary slot
Bootloader chainload address offset: 0x40000
Reset_Handler address offset: 0x40400
Jumping to the image
Booting the primary slot - flash remapping is disabled
*************************************
* Basic MCUBoot application example *
*************************************
$ image
Image 0; name APP; state None:
Slot 0 APP_PRIMARY; offset 0x0; size 0x100000 (1038576):
<IMAGE: size 28828; version 1.0.0+1000>
SHA256 of image payload: E069B6127A708EE88B39...
log_addr 0x0
*ACTIVE*
Slot 1 APP_SECONDARY; offset 0x100000; size 0x100000 (1038576):
<No Image Found>
$ image erase
Erasing inactive slot...done
$ xmodem_sb3
Started xmodem processing SB3
Make sure this device is provisioned to accept secure binary and its load address is 0x100000
Initiated XMODEM-CRC transfer. Receiving... (Press 'x' to cancel)
CCCCC
Received 51200 bytes
SB3 has been processed
$
$ image test
write magic number offset = 0x43ff00
$ reboot
System reset!
hello sbl.
Bootloader Version 2.2.0
Primary slot: version=1.0.0+1000
Secondary slot: version=1.1.0+1000
writing copy_done; fa_id=1 off=0x1fffe0 (0x43ffe0)
Image 0 loaded from the secondary slot
Bootloader chainload address offset: 0x240000
Reset_Handler address offset: 0x240400
Jumping to the image
Booting the secondary slot - flash remapping is enabled
*************************************
* Basic MCUBoot application example *
*************************************
$ image
Flash REMAP_SWAP active.
Image 0; name APP; state Testing:
Slot 0 APP_PRIMARY; offset 0x0; size 0x100000 (1038576):
<IMAGE: size 28828; version 1.0.0+1000>
SHA256 of image payload: E069B6127A708EE88B39...
log_addr 0x0 remaps to 0x100000
Slot 1 APP_SECONDARY; offset 0x100000; size 0x100000 (1038576):
<IMAGE: size 28828; version 1.1.0+1000>
SHA256 of image payload: E069B6127A708EE88B39...
log_addr 0x100000 remaps to 0x0
*ACTIVE*
$ image accept
$ image
Flash REMAP_SWAP active.
Image 0; name APP; state Permanent:
Slot 0 APP_PRIMARY; offset 0x0; size 0x100000 (1038576):
<IMAGE: size 28828; version 1.0.0+1000>
SHA256 of image payload: E069B6127A708EE88B39...
log_addr 0x0 remaps to 0x100000
Slot 1 APP_SECONDARY; offset 0x100000; size 0x100000 (1038576):
<IMAGE: size 28828; version 1.1.0+1000>
SHA256 of image payload: E069B6127A708EE88B39...
log_addr 0x100000 remaps to 0x0
*ACTIVE*
$