els_pkc_asymmetric#
Overview#
The ELS PKC application provides examples which demonstrate usage of most available algorithms and a crypto library lightweight testing:
AES-128/192/256 encryption/decryption, modes ECB/CBC/CTR/GCM/CMAC
SHA2-224/256/384/512 (including sha-direct mode)
KDF: CKDF (NIST SP 800-108 / SP800-56C), HKDF (RFC5869)
HMAC
ECC Sign/Verify/Keygen/Keyexchange (P-256)
RFC3394 key wrapping/unwrapping
Key Import/Export/Utilities/Provisioning
Random number Generation (DRBG/PRNG)
Supported Boards#
FRDM-MCXN236
Hardware requirements
Type-C USB cable
FRDM-MCXN236 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a type-c USB cable between the host PC and the MCU-Link USB port (J10) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
FRDM-MCXN947
Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
FRDM-MCXN947T
Hardware requirements
Type-C USB cable
FRDM-MCXN947T board
Personal Computer
Board settings
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
FRDM-RW612
Hardware requirements
Micro USB cable
FRDM-RW612 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the terminal will display similar information like the following:
ELS PKC asymmetric cipher example
============================ PKC ECC keygen sign verify:pass PKC RSA no-verify:pass PKC RSA sign no-encode:pass PKC RSA-PSS sign SHA256:pass PKC RSA-PSS verify SHA256:pass PKC ECC Curve25519:pass TLS Master session keys:pass
============================ RESULT: All 7 test PASS!! ELS example END
LPCXpresso55S36
Hardware requirements
Mini/micro USB cable
LPCXpresso55S36 board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the ELS (Crypto Sub System) and PKC (Public-Key Crypto Coprocessor) demo in the terminal window:
ELS PKC asymmetric cipher example
============================
PKC ECC keygen sign verify:pass
PKC RSA no-verify:pass
PKC RSA sign no-encode:pass
PKC RSA-PSS sign SHA256:pass
PKC RSA-PSS verify SHA256:pass
TLS Master session keys:pass
============================
RESULT: All 6 test PASS!!
ELS example END
MCX-N5XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
MCX-N9XX-EVK
Hardware requirements
Mini/micro USB cable
MCX-N9XX-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J5) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the hello world demo in the terminal window:
MIMXRT700-EVK
Hardware requirements
Micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the ELS (Crypto Sub System) and PKC (Public-Key Crypto Coprocessor) demo in the terminal window:
ELS PKC asymmetric cipher example
============================
PKC ECC keygen sign verify:pass
PKC RSA no-verify:pass
PKC RSA sign no-encode:pass
PKC RSA-PSS sign SHA256:pass
PKC RSA-PSS verify SHA256:pass
PKC ECC Curve25519:pass
TLS Master session keys:pass
============================
RESULT: All 7 test PASS!!
ELS example END
FRDM-IMXRT700
Hardware requirements
Type-C USB cable
FRDM-IMXRT700 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the CMSIS DAP USB port on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the ELS (Crypto Sub System) and PKC (Public-Key Crypto Coprocessor) demo in the terminal window:
ELS PKC asymmetric cipher example
============================
PKC ECC keygen sign verify:pass
PKC RSA no-verify:pass
PKC RSA sign no-encode:pass
PKC RSA-PSS sign SHA256:pass
PKC RSA-PSS verify SHA256:pass
PKC ECC Curve25519:pass
TLS Master session keys:pass
============================
RESULT: All 7 test PASS!!
ELS example END
RD-RW612-BGA
Hardware requirements
Micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the terminal will display similar information like the following:
ELS PKC asymmetric cipher example
============================ PKC ECC keygen sign verify:pass PKC RSA no-verify:pass PKC RSA sign no-encode:pass PKC RSA-PSS sign SHA256:pass PKC RSA-PSS verify SHA256:pass PKC ECC Curve25519:pass TLS Master session keys:pass
============================ RESULT: All 7 test PASS!! ELS example END