MCUXpresso SDK Documentation

ele_hseb_demo_secondary_core

ele_hseb_demo_secondary_core#

Overview#

This example provides a reference for setting up the default ele_hseb_demo application on the second core on multicore HSE-B-enabled devices.

The application is identical to ele_hseb_demo with the difference that it is executed from the secondary core. The devices, on which this example runs, are not enabled to run the secondary core independently. The role of the primary core application is to release the secondary core to run its application. A code snippet is provided to showcase such a release without the use of the multicore manager middleware.

Running the demo#

Example output on terminal:

* ELE_HSEB Demo started *

Check if HSEB FW is installed...HSEB FW is installed
Get FW version...Sucess

Check if NVM and RAM key catalogs are formatted...Key catalogs are formatted
Import symmetric keys for cryptographic operation...Success
Try erase keys...Success

Check if NVM and RAM key catalogs are formatted...Key catalogs are not formatted
Formatting key catalogs...Success
Import symmetric keys for cryptographic operation...Success

Exercise crypto operations:
AES crypto - passed
HASH crypto - passed
Session key - passed
Sys authorization - passed
NVM key update - passed
AES get key info - passed
RSA crypto - passed
AEAD crypto - passed

All tests passed!!
Demo end

Supported Boards#

FRDM-MCXE32B
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXE32B board

  • Personal Computer

Board settings
ELE HSEB Firmware Installation Guide

Before using ELE HSEB, you must first install the ELE HSEB Firmware to your device.

For detailed instructions on firmware installation, please refer to the firmware README file. The relative path points to the edgelock firmware release repository that should be available in your SDK at <sdk-root>/firmware/edgelock/.

Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.