lpspi_loopback#
Overview#
The lpspi_loopback demo shows how the lpspi do a loopback transfer, LPSPI master will transmit data to itself, so please connect the SOUT pin to SIN pin directly.
Running the demo#
When the example runs successfully, you can see the similar information from the terminal as below.
LPSPI functional interrupt example start. This example use one lpspi instance as master and another as slave on one board. Master uses interrupt way and slave uses interrupt way. Note that some LPSPI instances interrupt is in INTMUX ,you should set the intmux when you porting this example accordingly Please make sure you make the correct line connection. Basically, the connection is: LPSPI SOUT – SIN
LPSPI loopback example start LPSPI loopback test pass!!!
Supported Boards#
FRDM-MCXC353
Hardware requirements
Type-C USB cable
FRDM-MCXC353 board
Personal Computer
Board settings
LPSPI:
SPI0 connect to SPI0
Pin Name Board Location Pin Name Board Location
SOUT P1-0(J1A13) SIN P1-2(J1D2)
Prepare the Demo
Connect a USB Type-C cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal on PC for MCU-Link serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
***LPSPI Loopback Demo***
LPSPI loopback test pass!!!