MCUXpresso SDK Documentation

dma_linked_transfer

dma_linked_transfer#

Overview#

The DMA linked example is a simple demonstration program that uses the SDK software. It executes linked transfer(ping pong case) from the source buffer to destination buffer using the SDK DMA drivers.

Two descriptors are used, A is linked to B, B is linked to A.

A------>B------->
^               |
|               |
---------<-------

The purpose of this example is to show how to use the DMA and to provide a simple example for debugging and further development.

Supported Boards#

EVK-MIMXRT595
ardware requirements
  • Micro USB cable

  • EVK-MIMXRT595 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J40) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
EVK-MIMXRT685
ardware requirements
  • Micro USB cable

  • EVK-MIMXRT685 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
FRDM-MCXW23
Hardware requirements
  • Type-C USB cable

  • FRDM-MCXW23 Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the FRDM board J10.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
FRDM-RW612
ardware requirements
  • Micro USB cable

  • FRDM-RW612 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J10) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
LPC845BREAKOUT
Hardware requirements
  • Micro USB cable

  • LPC845 Breakout board

  • Personal Computer

Board settings

No special settings are required.

Prepare the demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port on the board.

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44
LPCXpresso51U68
Hardware requirements
  • Micro USB cable

  • LPCXpresso51U68 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J6) on the board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44
LPCXpresso54628
Hardware requirements
  • Micro USB cable

  • LPCXpresso54628 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44
LPCXpresso54S018
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44
LPCXpresso54S018M
Hardware requirements
  • Micro USB cable

  • LPCXpresso54S018M board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a micro USB cable between the host PC and the LPC-Link USB port (J8) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44
LPCXpresso55S06
ardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S06 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
LPCXpresso55S16
ardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S16 board

  • Personal Computer

Board settings

The jumper setting: Default jumpers configuration does not work, you will need to add JP20 and JP21 (JP22 optional for ADC use)

Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
LPCXpresso55S28
ardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S28 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44	111	222	333	444
LPCXpresso55S36
ardware requirements
  • Mini/micro USB cable

  • LPCXpresso55S36 board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J1) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
LPCXpresso55S69
ardware requirements
  • Mini/micro USB cable

  • LPCXpresso55s69 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

Note: MCUXpresso IDE project default debug console is semihost

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (P6) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44	111	222	333	444
LPCXpresso824MAX
Functional description

This example shows the usage of more than one descriptors to define a complicated transfer.

Hardware Requirements
  • Mini/micro USB cable

  • LPCXpresso824MAX board

  • Personal Computer

Board Settings

No special settings are required.

Run the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP port(J3 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the

    [Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).

  4. Launch the debugger in your IDE to begin running the demo.

Expected Result

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44
LPCXpresso845MAX
Functional description

This example shows the usage of more than one descriptors to define a complicated transfer.

Hardware Requirements
  • Mini/micro USB cable

  • LPCXpresso845MAX board

  • Personal Computer

Board Settings

No special settings are required.

Run the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP port(J4 on the board).

  2. Open a serial terminal with the following settings:

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Choose an IDE, building the project and download the program to the target board. More information about how to compile and program the project can refer to the

    [Getting Started with MCUXpresso SDK](../../../../docs/Getting Started with MCUXpresso SDK.pdf).

  4. Launch the debugger in your IDE to begin running the demo.

Expected Result

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.

Destination Buffer:

0   0   0   0   0   0   0   0

DMA linked transfer example finish.

Destination Buffer:

1   2   3   4   11  22  33  44
LPCXpresso860MAX
ardware requirements
  • Micro USB cable

  • LPCXpresso860MAX board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J4) on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 9600 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
MIMXRT685-AUD-EVK
ardware requirements
  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
RD-RW612-BGA
ardware requirements
  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings
Prepare the Demo
  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44
MCXW23-EVK
Hardware requirements
  • Mini/micro USB cable

  • MCXW23-EVK Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the EVK board J33.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA linked transfer example begin.
Destination Buffer:
0	0	0	0	0	0	0	0
DMA linked transfer example finish.
Destination Buffer:
1	2	3	4	11	22	33	44