MCUXpresso SDK Documentation

edma4_scatter_gather

edma4_scatter_gather#

Overview#

The EDMA memory to memory example is a simple demonstration program thatuses the SDK software. It executes one shot transfer from source buffer todestination buffer using the SDK EDMA drivers. The purpose of this example is to show how to use the EDMA and to provide a simple example for debugging and further development.

Supported Boards#

MIMXRT1180-EVK
Hardware requirements
  • Mini/micro USB cable

  • MIMXRT1180-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
MCIMX93AUTO-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93AUTO-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
MCIMX93-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
MCIMX93W-EVK
Hardware requirements
  • USB Type-C cable

  • MCIMX93W-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
MCIMX93-QSB
Hardware requirements
  • USB Type-C cable

  • MCIMX93-QSB board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
IMX943-EVK
Hardware requirements
  • Mini/micro USB cable

  • IMX943-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either re-power up your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
MIMXRT700-EVK
Hardware requirements
  • Micro USB cable

  • MIMXRT700-EVK board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
FRDM-IMXRT700
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT700 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the MCU-LINK USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
FRDM-MCXE31B
Hardware requirements
  • Micro USB cable

  • FRDM-MCXE31B Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
FRDM-MCXE32B
Hardware requirements
  • Micro USB cable

  • FRDM-MCXE32B board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a type-c USB cable between the host PC and the MCU-Link USB port (J13) on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8
FRDM-IMXRT1186
Hardware requirements
  • Type-C USB cable

  • FRDM-IMXRT1186 board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo
  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EDMA scatter_gather example begin.

Destination Buffer:
0       0       0       0       0       0       0       0

EDMA scatter_gather example finish.

Destination Buffer:
1       2       3       4       5       6       7       8