Flow – ram_only Debug#
ram_only Debug#
Step 1. Install debug patch
(see Patch Install section)
Step 2. Set boot switch to 0b00 (XSPI NOR boot mode)
Step 3. Build with ram_only target
Step 4. Connect debugger
Step 5. Download ELF to ITCM and debug
--> DONE
POR boot: the image downloaded by the debugger is volatile and does not POR boot. To create a POR-bootable image, a boot header must be attached – either at build time or via an external tool. Refer to the RAM ONLY Targets section of this guide for details.