Wireless connectivity middleware overview#
Component versions:
Wireless connectivity component |
Version |
|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
The following connectivity-supporting documentation is included with this release:
Bluetooth Low Energy Quick Start Guide
Bluetooth Low Energy Demo Applications User’s Guide
Bluetooth Low Energy Application Developer’s Guide
Bluetooth Low Energy Host Stack API Reference Manual
Bluetooth Low Energy Host Stack FSCI Application Programming
Bluetooth Low Energy Host Stack FSCI Reference Manual
Bluetooth Low Energy Connection Handover
Bluetooth Low Energy Localization Application Note
Bluetooth Low Energy Channel Sounding Application Developers Guide
Bluetooth Channel Sounding Technique for Distance Estimation
CS Wireless Ranging Demo Application User Guide
Generic FSK Link Layer Quick Start Guide
Generic FSK Link Layer API Reference Manual
Connectivity Framework Reference Manual
Connectivity Framework API Documentation
Low Power Connectivity Reference Design User’s Guide
Zigbee Demo Applications User Guide
ZigBee 3.0 Stack User Guide
ZigBee Cluster Library User Guide
ZigBee 3.0 Devices User Guide
Zigbee Green Power User Guide
Zigbee Core Utilities User Guide
IEEE 802.15.4 Connectivity Test Application Getting Started Guide
IEEE 802.15.4 Connectivity Test Application Command Line Interface User Guide
Bluetooth LE Host Stack and Applications#
The Bluetooth LE Host Stack component provides an implementation for a Bluetooth 6.0 mandatory and some optional, proprietary, and experimental features. The Bluetooth LE Host Stack component provides application examples, services, and profiles.
Main features supported:
Automotive Compliance
MISRA Compliance
HIS CCM <= 20
Advanced Secure Mode
Enhanced ATT
GATT Caching
GCC Libraries
IAR Libraries
Bluetooth LE Peripheral Libraries
Bluetooth LE Central Libraries
Bluetooth LE Full Host Features Libraries
Bluetooth LE Host Optional Features Libraries
Bluetooth LE Host Mandatory Features Libraries
BareMetal and FreeRTOS Support
Full Privacy Support
NCP Mode - FSCI Application
Enhanced Notifications
Dynamic Database
OTA Support - Sample Applications
Decision based Advertising Filtering (DBAF)
Advertising Coding Selection (ACS)
Periodic Advertising with Responses (PAwR)
Encrypted Advertising Data (EAD)
Monitoring Advertisers - Experimental feature
Randomized RPA - Experimental feature
LE Enhanced Connection Update - Experimental feature
Intrusion Detection System (IDS)
Note: The CDE (Complex-domain Distance Estimation) algorithm is an experimental feature intended only for testing purposes. It is not maintained and must not be included in the production environments.
Bluetooth LE Controller#
Refer to the Bluetooth LE Controller release notes in the middleware documentation.
IEEE 802.15.4#
Refer to the IEEE 802.15.4 release notes in the middleware documentation.
XCVR#
Refer to the XCVR release notes in the middleware documentation.
GenFSK Link Layer#
Refer to the GenFSK Link Layer release notes in the middleware documentation.
Low Power Reference Design Applications#
Refer to the Low Power Reference Design release notes in the middleware documentation.
Zigbee#
Refer to the Zigbee release notes in the middleware documentation.
Connectivity Framework#
Refer to the Connectivity Framework release notes in the middleware documentation.
Parent topic:Middleware