How to set the board to the Bootloader ISP mode#
On the MCX-W72-EVK board:
Press and hold the BOOT CONFIG switch, SW4.
Connect the MCX-W72-EVK board via the micro-USB connector to the PC.
Release the switch SW4.
Check the associated USB port number on the PC (such as COM10).
While the MCXW72 is in bootloader ISP mode, navigate to the folder where blhost.exe is located.
Type the command
.\blhost.exe -p COM10 -- get-property 1to make sure that the MCXW72 is in Bootloader ISP mode, you should see:Ping responded in 1 attempt(s)
Inject command ‘get-property’
Response status = 0 (0x0) Success.
Response word 1 = 1258488064 (0x4b030100)
Current Version = K3.1.0
On a custom board:
Short the
BOOT_CFGpin to VDD while reset.