ZPS_eAplZdpRemoveNodeCacheRequest
ZPS\_teStatus ZPS\_eAplZdpRemoveNodeCacheRequest\(
PDUM\_thAPduInstance hAPduInst,
ZPS\_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS\_tsAplZdpRemoveNodeCacheReq
*psZdpRemoveNodeCacheReq);
Description
This function requests a Primary Discovery Cache node to remove from its cache all ‘discovery information’ relating to a particular End Device. The function sends a Remove_node_cache_req request to the Primary Discovery Cache node.
The effect of a successful request is to remove the relevant ‘discovery information’ and free the corresponding storage space in the cache previously reserved by ZPS_eAplZdpDiscoveryStoreRequest()\ (which may have been called from another node in the network).
This request includes the network and IEEE addresses of the End Device whose ‘discovery information’ is to be removed. The request is represented by the structure below (further detailed in Section 9.2.2.22).
typedef struct {
uint16 u16NwkAddr;
uint64 u64IeeeAddr;
} ZPS_tsAplZdpRemoveNodeCacheReq;
On receiving the request, the remote node first checks whether it has a primary discovery cache. If this is the case, it checks whether it has previously received and implemented a Discovery_store_reqrequest for the specified End Device, resulting from a call to ZPS_eAplZdpDiscoveryStoreRequest(). If it has, it deletes the relevant data and unreserve the corresponding part of the cache.
The node replies with a Remove_node_cache_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpRemoveNodeCacheRsp(detailed in Section 9.2.3.21).
Parent topic:ZPS_eAplZdpRemoveNodeCacheRequest
Parameters
hAPduInst: Handle of APDU instance in which request is sent.
uDstAddr: Address of destination node of request(can be 16- or 64-bit, as specified by bExtAddr)
bExtAddr: Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
*pu8SeqNumber: Pointer to sequence number of request
*psZdpRemoveNodeCacheReq: Pointer to request (see above)
Parent topic:ZPS_eAplZdpRemoveNodeCacheRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpRemoveNodeCacheRequest
Parent topic:Service Discovery functions