ZPS_eAplZdpRemoveBkupBindEntryRequest
ZPS_teStatus ZPS_eAplZdpRemoveBkupBindEntryRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpRemoveBkupBindEntryReq
*psZdpRemoveBkupBindEntryReq);
Description
This function requests the removal of an entry in the back-up binding table cache on a remote node. The function must be called from the node with the corresponding primary binding table cache. The removal of a back-up entry is normally required when an entry in the primary binding table cache has been removed.
Note: This function is provided in the NXP ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.
This request must include the binding table entry to be removed. The request is represented by the structure below (further detailed in Section 9.2.2.28).
typedef struct {
uint64 u64SrcAddress; uint8 u8SrcEndPoint; uint16 u16ClusterId; uint8 u8DstAddrMode; union {
struct {
uint16 u16DstAddress;
} sShort; struct {
uint64 u64DstAddress; uint8 u8DstEndPoint;
} sExtended;
};
} ZPS_tsAplZdpRemoveBkupBindEntryReq;
On receiving the request, the remote node removes the specified binding table entry from its back-up binding table cache, if possible.
The remote node replies with a Remove_Bkup_Bind_Entry_rsp response, which should be collected using the function **ZQ_bZQueueReceive()**and stored in a structure of type ZPS_tsAplZdpRemoveBkupBindEntryRsp(detailed in Section9.2.3.28).
Parent topic:ZPS_eAplZdpRemoveBkupBindEntryRequest
Parameters
hAPduInst Handle of APDU instance in which request is sent.
uDstAddr Address of destination node of request (can be 16- or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpRemoveBkupBindEntryReq Pointer to request (see above)
Parent topic:ZPS_eAplZdpRemoveBkupBindEntryRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpRemoveBkupBindEntryRequest
Parent topic:Binding functions