MCUXpresso SDK Release Notes
Overview
The MCUXpresso SDK is a comprehensive software enablement package designed to simplify and accelerate application development with Arm Cortex-M-based devices from NXP, including its general purpose, crossover and Bluetooth-enabled MCUs. MCUXpresso SW and Tools for DSC further extends the SDK support to current 32-bit Digital Signal Controllers. The MCUXpresso SDK includes production-grade software with integrated RTOS (optional), integrated enabling software technologies (stacks and middleware), reference software, and more.
In addition to working seamlessly with the MCUXpresso IDE, the MCUXpresso SDK also supports and provides example projects for various toolchains. The Development tools chapter in the associated Release Notes provides details about toolchain support for your board. Support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
Underscoring our commitment to high quality, the MCUXpresso SDK is MISRA compliant and checked with Coverity static analysis tools. For details on MCUXpresso SDK, see MCUXpresso-SDK: Software Development Kit for MCUXpresso.
MCUXpresso SDK
As part of the MCUXpresso software and tools, MCUXpresso SDK is the evolution of Kinetis SDK, includes support for LPC, DSC,PN76, and i.MX System-on-Chip (SoC). The same drivers, APIs, and middleware are still available with support for Kinetis, LPC, DSC, and i.MX silicon. The MCUXpresso SDK adds support for the MCUXpresso IDE, an Eclipse-based toolchain that works with all MCUXpresso SDKs. Easily import your SDK into the new toolchain to access to all of the available components, examples, and demos for your target silicon. In addition to the MCUXpresso IDE, support for the MCUXpresso Config Tools allows easy cloning of existing SDK examples and demos, allowing users to leverage the existing software examples provided by the SDK for their own projects.
In order to maintain compatibility with legacy Freescale code, the filenames and source code in MCUXpresso SDK containing the legacy Freescale prefix FSL has been left as is. The FSL prefix has been redefined as the NXP Foundation Software Library.
Development tools
The MCUXpresso SDK was tested with following development tools. Same versions or above are recommended.
MCUXpresso IDE, Rev. 25.06.xx
IAR Embedded Workbench for Arm, version is 9.60.4
Keil MDK, version is 5.41
MCUXpresso for VS Code v25.06
GCC Arm Embedded Toolchain 14.2.x
Supported development systems
This release supports board and devices listed in following table. The board and devices in bold were tested in this release.
Development boards |
MCU devices |
|---|---|
FRDM-RW612 |
RW610ETA2I, RW610HNA2I, RW610UKA2I, |
MCUXpresso SDK release package
The MCUXpresso SDK release package content is aligned with the silicon subfamily it supports. This includes the boards, CMSIS, devices, middleware, and RTOS support.
Device support
The device folder contains the whole software enablement available for the specific System-on-Chip (SoC) subfamily. This folder includes clock-specific implementation, device register header files, device register feature header files, and the system configuration source files. Included with the standard SoC support are folders containing peripheral drivers, toolchain support, and a standard debug console. The device-specific header files provide a direct access to the microcontroller peripheral registers. The device header file provides an overall SoC memory mapped register definition. The folder also includes the feature header file for each peripheral on the microcontroller. The toolchain folder contains the startup code and linker files for each supported toolchain. The startup code efficiently transfers the code execution to the main() function.
Board support
The boards folder provides the board-specific demo applications, driver examples, and middleware examples.
Demo application and other examples
The demo applications demonstrate the usage of the peripheral drivers to achieve a system level solution. Each demo application contains a readme file that describes the operation of the demo and required setup steps. The driver examples demonstrate the capabilities of the peripheral drivers. Each example implements a common use case to help demonstrate the driver functionality.
RTOS
FreeRTOS
Real-time operating system for microcontrollers from Amazon
Middleware
CMSIS DSP Library
The MCUXpresso SDK is shipped with the standard CMSIS development pack, including the prebuilt libraries.
memfault-firmware-sdk
memfault-firmware-sdk
Wireless Connectivity Framework
The Connectivity Framework is a software component that provides hardware abstraction modules to the upper layer connectivity stacks and components. It also provides a list of services and APIs, such as, Low power, Over the Air (OTA) Firmware update, File System, Security, Sensors, Serial Connectivity Interface (FSCI), and others. The Connectivity Framework modules are located in the middleware\wireless\framework SDK folder.
wpa_supplicant-rtos
NXP Wi-Fi WPA Supplicant
Wireless EdgeFast Bluetooth PAL
For more information, see the MCUXpresso SDK EdgeFast Bluetooth Protocol Abstraction Layer User’s Guide.
Ethermind BT/BLE Stack
nxp_bt_ble_stack
coreHTTP
coreHTTP
NXP Wi-Fi
The MCUXpresso SDK provides driver for NXP Wi-Fi external modules. The Wi-Fi driver is integrated with LWIP TCPIP stack and demonstrated with several network applications (iperf and AWS IoT).
For more information, see Getting Started with NXP based Wireless Modules and i.MX RT Platform Running on RTOS (document: UM11441).
USB Type-C PD Stack
See the MCUXpresso SDK USB Type-C PD Stack User’s Guide (document MCUXSDKUSBPDUG) for more information
USB Host, Device, OTG Stack
See the MCUXpresso SDK USB Stack User’s Guide (document MCUXSDKUSBSUG) for more information.
TinyCBOR
Concise Binary Object Representation (CBOR) Library
TF-M
Trusted Firmware - M Library
PSA Test Suite
Arm Platform Security Architecture Test Suite
Mbed Crypto
Mbed Crypto library
PKCS#11
The PKCS#11 standard specifies an application programming interface (API), called “Cryptoki,” for devices that hold cryptographic information and perform cryptographic functions. Cryptoki follows a simple object based approach, addressing the goals of technology independence (any kind of device) and resource sharing (multiple applications accessing multiple devices), presenting to applications a common, logical view of the device called a “cryptographic token”.
NXP IoT Agent
NXP IoT Agent
MCU Boot
Open source MCU Bootloader.
mbedTLS
mbedtls SSL/TLS library v3.x
mbedTLS
mbedtls SSL/TLS library v2.x
Voice Seeker (no AEC)
VoiceSeeker is a multi-microphone voice control audio front-end signal processing solution. VoiceSeeker is not featuring acoustic echo cancellation (AEC).
lwIP
The lwIP TCP/IP stack is pre-integrated with MCUXpresso SDK and runs on top of the MCUXpresso SDK Ethernet driver with Ethernet-capable devices/boards.
For details, see the lwIP TCPIP Stack and MCUXpresso SDK Integration User’s Guide (document MCUXSDKLWIPUG).
lwIP is a small independent implementation of the TCP/IP protocol suite.
LVGL
LVGL Open Source Graphics Library
llhttp
HTTP parser llhttp
LittleFS
LittleFS filesystem stack
FreeMASTER
FreeMASTER communication driver for 32-bit platforms.
File systemFatfs
The FatFs file system is integrated with the MCUXpresso SDK and can be used to access either the SD card or the USB memory stick when the SD card driver or the USB Mass Storage Device class implementation is used.
cJSON
Ultralightweight JSON parser in ANSI C
AWS IoT
Amazon Web Service (AWS) IoT Core SDK.
NXP PSA CRYPTO DRIVER
PSA crypto driver for crypto library integration via driver wrappers
NXP ELS PKC
ELS PKC crypto library
Release contents
Provides an overview of the MCUXpresso SDK release package contents and locations.
Deliverable |
Location |
|---|---|
Boards |
INSTALL_DIR/boards |
Demo Applications |
INSTALL_DIR/boards/<board_name>/demo_apps |
Driver Examples |
INSTALL_DIR/boards/<board_name>/driver_examples |
eIQ examples |
INSTALL_DIR/boards/<board_name>/eiq_examples |
Board Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/boards/<board_name>/project_template |
Driver, SoC header files, extension header files and feature header files, utilities |
INSTALL_DIR/devices/<device_name> |
CMSIS drivers |
INSTALL_DIR/devices/<device_name>/cmsis_drivers |
Peripheral drivers |
INSTALL_DIR/devices/<device_name>/drivers |
Toolchain linker files and startup code |
INSTALL_DIR/devices/<device_name>/<toolchain_name> |
Utilities such as debug console |
INSTALL_DIR/devices/<device_name>/utilities |
Device Project Template for MCUXpresso IDE NPW |
INSTALL_DIR/devices/<device_name>/project_template |
CMSIS Arm Cortex-M header files, DSP library source |
INSTALL_DIR/CMSIS |
Components and board device drivers |
INSTALL_DIR/components |
RTOS |
INSTALL_DIR/rtos |
Release Notes, Getting Started Document and other documents |
INSTALL_DIR/docs |
Tools such as shared cmake files |
INSTALL_DIR/tools |
Middleware |
INSTALL_DIR/middleware |
Known issues
This section lists the known issues, limitations, and/or workarounds.
SDK does not fully support the MCUX Config Tool
Currently, the pin/clock config files in the MCUXpresso SDK are not generated from the MCUXpresso Config Tool. As a result, there is an error reported during project import/clone from the SDK package. However, the Config Tool itself can work without any issue
Cloned project cannot build issue
Some cloned projects cannot build due to missing dependent component configuration. To fix the issue, you must correct the configuration manually in the cloned project.
The failed projects include nbu_bb_bm, wifi_cli_over_ble_wu, and ncp_device.
Romapi_flexspi example not working
The romapi_flexspi example fails to work with armgcc flash_debug target.
No UART simulated for hello_world_virtual_com
No UART peripheral is simulated for hello_world_virtual_com after downloading.
Limitations when creating a new FreeRTOS-based C/C++ project
Due to the missing component dependencies definition, there are several limitations when creating a new FreeRTOS-based C/C++ project in MCUXpresso IDE. When the FreeRTOS kernel component is selected (under Operating Systems/RTOS/Core menu), you must manually select the FreeRTOS cm33 non trustzone port component (under Middleware/RTOS menu) for projects without TrustZone. For FreeRTOS TrustZone projects creation, the support is not ready.
GPIO toggle operation not working on NCP SPI slave side with flash release build
Due to IDE compile optimization for the flash release target, the GPIO toggle operation on the NCP SPI slave side to indicate RX DMA ready or slave to master transfer is not working. The issue occurs because the GPIO toggle time is too short for the host to detect it.
El2go_agent_demo_wifi issue
The el2go_agent_demo_wifi project does not work on MCUXpresso for VSCode. However, Arm GCC standalone, MCUXpresso IDE, MDK, or IAR have no limitations.
Note: The above issue is not really a limitation of the SDK release, as it gets fixed by a toolchain update. The issue also partially applies to all other examples using TF-M.
When using MCUX IDE, do not specify a custom prefix or suffix while importing the example.
However, if it is a custom prefix or suffix is added, you must adapt the names of the library projects el2go_mbedtls_lib and el2go_tfm_psa_ns_lib in the el2go_agent_demo_wifi_ns project. To change the linker import paths to the right name, select Project settings > C/C++ Build > Settings > MCU linker > Miscellaneous > Other Objects.
Note: This limitation stays as it depends on the SDK generator fixes
Example mbedtls_benchmark may hang on some targets on devices with ELS acceleration
Some targets of ELS accelerated devices may experience runtime issues when run with the default configuration of the mbedtls_benchmark application.
Examples: mbedtls_benchmark
Affected toolchains: All
The freertos_lpuart example does not complete successfully
The example hangs after console output ‘FreeRTOS LPUART driver example’.
Examples: freertos_lpuart
Affected toolchains: All
The example does not perform as expected (Ticks do not printed on the console or the application does not wake up from the sleep mode).
Examples: freertos_tickless
Affected toolchains: All
TF-M secure and EL2GO examples incorrect path in “Download extra image” with iar and mdk IDEs with Kex package
TF-M secure and EL2GO examples are missing the target path for ns binary in “extra download image” with iar and mdk IDEs
Examples: tfm_demo_s, tfm_psatest_s, tfm_regression_s, tfm_secureboot_s, el2go_agent_s, el2go_blob_test_s, el2go_import_blob_s, el2go_mqtt_demo_s Affected toolchains: mdk, iar Affected platforms: mcxn5xxevk, frdmmcxn947, mcxn9xxevk, rdrw612bga, frdmrw612 Workaround: There are two ways 1.) Flash secure and non secure bins via Jlink or SPSDK after the build with IDE and providing with correct paths of secure and non-secure binaries. or 2.) Add {target} debug/release in path of “Download extra image” for iar and for MDK in xxx_flashdownload.ini file.