coreHTTP Client Library
This repository contains a C language HTTP client library designed for embedded platforms. It has no dependencies on any additional libraries other than the standard C library, llhttp, and a customer-implemented transport interface. This library is distributed under the MIT Open Source License.
This library has gone through code quality checks including verification that no function has a GNU Complexity score over 8. This library has also undergone both static code analysis from Coverity static analysis, and validation of memory safety and data structure invariance through the CBMC automated reasoning tool.
See memory requirements for this library here.
coreHTTP v3.0.0 source code is part of the FreeRTOS 202210.00 LTS release.
coreHTTP v2.0.0 source code is part of the FreeRTOS 202012.00 LTS release.
coreHTTP Config File
The HTTP client library exposes configuration macros that are required for
building the library. A list of all the configurations and their default values
are defined in core_http_config_defaults.h.
To provide custom values for the configuration macros, a custom config file
named core_http_config.h can be provided by the user application to the library.
By default, a core_http_config.h custom config is required to build the
library. To disable this requirement and build the library with default
configuration values, provide HTTP_DO_NOT_USE_CUSTOM_CONFIG as a compile time
preprocessor macro.
The HTTP client library can be built by either:
Defining a
core_http_config.hfile in the application, and adding it to the include directories for the library build. ORDefining the
HTTP_DO_NOT_USE_CUSTOM_CONFIGpreprocessor macro for the library build.
Building the Library
The httpFilePaths.cmake file contains the information of all source files and header include paths required to build the HTTP client library.
As mentioned in the previous section, either a custom
config file (i.e. core_http_config.h) OR HTTP_DO_NOT_USE_CUSTOM_CONFIG macro
needs to be provided to build the HTTP client library.
For a CMake example of building the HTTP library with the httpFilePaths.cmake
file, refer to the coverity_analysis library target in
test/CMakeLists.txt file.
Building Unit Tests
Platform Prerequisites
For running unit tests, the following are required:
C90 compiler like gcc
CMake 3.13.0 or later
Ruby 2.0.0 or later is required for this repository’s CMock test framework.
For running the coverage target, the following are required:
gcov
lcov
Steps to build Unit Tests
Go to the root directory of this repository.
Run the cmake command:
cmake -S test -B build -DBUILD_CLONE_SUBMODULES=ONRun this command to build the library and unit tests:
make -C build allThe generated test executables will be present in
build/bin/testsfolder.Run
cd build && ctestto execute all tests and view the test run summary.
CBMC
To learn more about CBMC and proofs specifically, review the training material here.
The test/cbmc/proofs directory contains CBMC proofs.
In order to run these proofs you will need to install CBMC and other tools by following the instructions here.
Reference examples
The AWS IoT Device SDK for Embedded C repository contains demos of using the HTTP client library here on a POSIX platform. These can be used as reference examples for the library API.
Documentation
Existing Documentation
For pre-generated documentation, please see the documentation linked in the locations below:
Location |
|---|
Note that the latest included version of coreHTTP may differ across repositories.
Generating Documentation
The Doxygen references were created using Doxygen version 1.9.2. To generate the Doxygen pages, please run the following command from the root of this repository:
doxygen docs/doxygen/config.doxyfile
Contributing
See CONTRIBUTING.md for information on contributing.