Hardware overview
This section provides information on hardware support and instructions to connect the CMWC1ZZABR-107-EVB adapter to the evaluation boards. The guide uses LPC55S69 as reference, but same steps apply to other supported products from the LPC55 family products.
Supported platforms
The SDK supports the following hardware:
LPCXpresso55S16
LPCXpresso55S28
LPCXpresso55S69
LPCXpresso55S3x/3x
EVK-MIMXRT1020
LPCXpresso54628
LPCXpresso54S018
LPCXpresso54S018M
Parent topic:Hardware overview
Assembly instructions
Mount the CMWC1ZZABR-107-EVB adapter to the mikroBUS connector on your board. Make sure that the pin labeling matches the pin orientation between the boards.
|
|
|

|
Parent topic:Hardware overview
Additional hardware
The additional hardware required includes:
USB A to micro USB cable
Personal computer
The Wi-Fi demo application does not require any special hardware configuration. However, when running the Wi-Fi demo, it is recommended to leave the development board jumper settings and configurations in the default state.
Parent topic:Hardware overview