SLIM feature {#topic_d2a98636-e88b-43ee-b8e4-c9be1a554855}
The SLIM feature is used to reduce the consumption of the flash memory and SRAM of low-end boards like the FRDM MCXN947.
Memory impact:
Maximum Flash usage: 607.62 KB (29.67%).
Maximum SRAM usage: 297.73 KB (58.15%)
SLIM macros |
Feature disabled |
|---|---|
CONFIG_WIFI_SLIM_ROAM |
CONFIG_ROAMING |
CONFIG_WIFI_SLIM_STA |
CONFIG_5GHz_SUPPORT\ (applicable for RW612) |
CONFIG_WIFI_SLIM_UAP |
CONFIG_UAP_STA_MAC_ADDR_FILTER |
CONFIG_FREERTOS_LOW_MEMORY_FOOTPRINT |
When the macro is enabled, the heap memory usage is reduced by 10 KB (from 70 KB to 60 KB). |
CONFIG_LWIP_LOW_MEM_FOOTPRINT |
When the macro is enabled:
|
Parent topic:Feature enable and memory impact