AP-STA mode {#topic_f7231db1-b1df-4e20-822f-02c97f3c11e8}
Features |
Sub features |
88W8987 |
IW416 |
IW611/IW612 |
RW610/RW612 |
AW611 |
88W8801 |
|---|---|---|---|---|---|---|---|
Simultaneous AP-STA operation (same channel) |
AP-STA functionality |
Y |
Y |
Y |
Y |
Y |
Y |
SAD |
Software antenna diversity |
Y |
Y |
Y |
Y |
Y |
Y |
Generic |
Firmware download (parallel)[^1] |
Y |
Y |
Y |
N |
Y |
N |
Generic |
Secure boot |
N |
N |
Y |
Y |
Y |
N |
Generic |
Slim feature |
N |
Y |
N |
Y |
N |
N |
Parent topic:Wi-Fi radio
[^1] Feature not enabled by default in the SDK. Refer to Feature enable and memory impact for the macro to enable the feature and the impact on the memory when enabling the feature.