dev_cdc_ecm_nic_lite_bm
Overview
The device CDC-ECM project is a simple demonstration program based on the MCUXpresso SDK. It is enumerated as an Ethernet network adapter and users can access the network using the adapter.
System Requirement
Hardware requirements
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements
The project path is:
MCUXpresso_SDK_Install/boards/board/usb_examples/usb_device_cdc_ecm_nic_lite/rtos/toolchain.
The
rtosmeans “Bare Metal” or “FreeRTOS OS”, in path, it is “bm” or “freertos”.
Getting Started
Hardware Settings
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
Download the program to the target board.
Connect the target board to the external power source (the example is self-powered).
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Connect a USB cable between the PC host and the USB device port on the board.
For PC host, this demo only support for Linux-like OS & Mac OS.
For detailed instructions, see the appropriate board User’s Guide.
Run the example
The demo will send string “USB CDC-ECM NIC Device” on the serial port to indicate that the USB CDC-ECM Device function is ready.
The PC enumerates the USB device normally and accesses the network via DHCP or manual configuration.
Supported Boards
FRDM-RW612