Hardware requirements
Mini/micro USB cable
EVK-MIMXRT1170 board
Personal Computer
SD card
Board settings
Please make sure R136 is weld for GPIO card detect.
Prepare the Demo
Connect a micro USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Insert SD card to card slot
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the terminal like:
Card size xxxxx bytes
Working condition:
  Voltage : xxxV
  Timing mode: xxx
  Freq : xxx HZ
Read/Write/Erase the card continuously until encounter error......
Write/read one data block......
Compare the read/write content......
The read/write content is consistent.
Write/read multiple data blocks......
Compare the read/write content......
The read/write content is consistent.
Erase multiple data blocks......
Input 'q' to quit read/write/erase process.
Input other char to read/write/erase data blocks again.