Sysbuild
Sysbuild is a higher-level build system that can be used to combine multiple other build systems together. It’s ported from Sysbuild (System build) — Zephyr Project. In MCUXpresso SDK build system, it’s mainly used for multi-project example build.
Sysbuild files
To include sub projects into building system, you must prepare sysbuild.cmake into main project folder. Sub projects can be located anywhere which are imported by ExternalMCUXProject_Add command inside sysbuild.cmake.
Take multicore hello_world for example:
# examples/multicore_examples/hello_world/primary/sysbuild.cmake
ExternalMCUXProject_Add(
APPLICATION hello_world_secondary_core
SOURCE_DIR ${APP_DIR}/../secondary
board ${SB_CONFIG_secondary_board}
core_id ${SB_CONFIG_secondary_core_id}
config ${SB_CONFIG_secondary_config}
toolchain ${SB_CONFIG_secondary_toolchain}
)
# Let's build the secondary application first
add_dependencies(${DEFAULT_IMAGE} hello_world_secondary_core)
The ${APP_DIR} means the build directory of primary project and ${DEFAULT_IMAGE} indicates the primary project target. The build sequence can be determined by add_dependencies function in sysbuild.cmake.
The variables with SB_ prefix in sysbuild.cmake can be defined before adding sub projects. Or you can pass them with west command -D.
In practice it is more common to set these variables automatically via kconfig to support multiple platforms in a more flexible way. For example, you can prepare a Kconfig.sysbuild in main project folder:
# examples/middleware/multicore/multicore_examples/hello_world/primary/Kconfig.sysbuild
config secondary_board
string
default "$(board)"
config secondary_core_id
string
default "cm4" if $(board) = "evkbmimxrt1170" && $(core_id) = "cm7"
default "cm33_core1" if $(board) = "lpcxpresso55s69" && $(core_id) = "cm33_core0"
config secondary_config
string
default "debug" if $(config) = "debug"
default "debug" if $(config) = "flexspi_nor_debug"
config secondary_toolchain
string
default "$(toolchain)"
Sysbuild is used to organize project build sequence, about how images are linked together is set by the project’s own CMakeLists.txt. For example, you must import the secondary core binary in the CMakeLists.txt of primary project:
# examples/multicore_examples/hello_world/secondary/CMakeLists.txt
mcux_convert_binary(
TOOLCHAINS armgcc mdk iar
BINARY ${APPLICATION_BINARY_DIR}/${CONFIG_TOOLCHAIN}/core1_image.bin
)
# examples/multicore_examples/hello_world/primary/CMakeLists.txt
mcux_add_iar_configuration(
LD "--image_input=${APPLICATION_BINARY_DIR}/../hello_world_secondary_core/iar/core1_image.bin,_core1_image, __core1_image,4 "
)
Build command
To enable sysbuild, only --sysbuild is needed when you build the main project:
west build -b evkbmimxrt1170 --sysbuild ./examples/multicore_examples/hello_world/primary -Dcore_id=cm7 --config flexspi_nor_debug --toolchain=armgcc -p always
Kconfig GUI
The sysbuild projects can be configured with Kconfig GUI just like a normal project in the build system. The only difference is the target name, for main project, they’re menuconfig or guiconfig, for sub project, you must add project name prefix to differ each target.
For example:
west build -t guiconfig
west build -t hello_world_secondary_core_guiconfig