Build an example application
To build the hello_world example application, perform the following example steps:
Launch CodeWarrior. In the workspace launcher, choose a workspace which holds the projects to use. If the dialogue box does not pop up, enter a workspace folder and create one workspace.
|

|
Then the CodeWarrior Development Studio workspace with empty projects appears.
|
|
Import the project into the workspace.
Click Import project in the Commander pane. A form pops up. Click Browse to the SDK install directory.
|

|
Then all available demo projects are as shown in [Figure 3](build_an_example_application.md#FIG_PROJECTIMPORT). Select the `hello_world` project in the list, and click **Finish**.
If you already know the project location, navigate to the folder when clicking **Browse**, and only one project can be seen.
To locate most example application workspace files, use the following path:
```
<install_dir>/boards/<board_name>/<example_type>/<application_name>/codewarrior
```
Using the MC56F81000-EVK hardware platform as an example, the `hello_world` workspace is located in:
```
<install_dir>/boards/evkmc56f81000/demo_apps/hello_world/codewarrior
```
Select the desired build target from the drop-down menu. For this example, select hello_world – flash_sdm_lpm_debug, as shown in Figure 4.
|

|
To build the demo application, click Build (All) in the Commander pane.
The build completes without errors.
Parent topic:Run a demo application using CodeWarrior