Other limitations
Documentation may not be fully updated to refer to KW47 devices.
GenFSK Connectivity_test application is not operational with ARMGCC compiler.
GenFSK
Connectivity_testapplication is not operational with Low Power enabled.Serial manager is only supported on UART (not I2C nor SPI).
The
--no-warn-rwx-segmentscannot been recognized on legacy MCUXpresso IDE versions.The
--no-warn-rwx-segmentsoption in MCUXpresso projects should be manually removed from the project settings if someone needs to use legacy (< 11.8.0) MCUXpresso IDE versionsIf the FRO32K is configured as the clock source of Core 0 then the debug session will stuck in both IAR, MCUX CMSIS-DAP while debugging. Use a lower debug wire speed, for example 1 MHz instead of the default one.
In IAR, the option is in Runtime Checking -> Debugger -> CMSIS DAP -> Interface -> Interface speed.
In MCUXpresso IDE, the option is in LinkServer Debugger -> Advanced Settings -> Wirespeed (Hz).
If the configuration tool is used to clone
tfm-relatedprojects, there is a problem that region_defs.h cannot be found in the cloned project.Not supported features:
Platform low power modes not fully enabled in this release.
FRO32K mode not fully supported in this release.
Low power reference design applications are not supported for the armgcc toolchain from zip archives. Please use MCUXpresso IDE or IAR toolchains for development using these applications.
Some connection events may be missed by the NBU core firmware when an asynchronous wake up is triggered from the application core.
Parent topic:Known issues