Build an example application
To build an example application, follow these steps.
Open the GCC Arm embedded toolchain command window. To launch the window on the Windows operating system, select Start -> Programs -> GNU Tools ARM Embedded <version> -> GCC Command Prompt.
|

|
Change the directory to the example application project directory, which has a path similar to the following:
<install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc
For this example, the exact path is:
<install_dir>/boards/evkmimx8ulp/demo_apps/hello_world/armgcc
Type
build_debug.batat the command-line or double-click thebuild_debug.batfile in Windows Explorer to perform the build. The output is as shown in Figure 2.|

|
Note: To run the application, see the Run an application using imx-mkimage.
Parent topic:Windows OS host