Maestro USB speaker example
Table of content
Overview {#maestro-usb-speaker-overview}
The Maestro USB speaker example demonstrates audio processing on the ARM cortex core utilizing the Maestro Audio Framework library.
The application is controlled by commands from a shell interface using serial console.
The development board will be enumerated as a USB audio class 2.0 device on the USB host. The application takes audio samples from the USB host and sends them to the audio Line-Out port. User will see the volume levels obtained from the USB host but this is only an example application. To leverage the volume values, the demo has to be modified.
Depending on target platform or development board there are different modes and features of the demo supported.
Standard - The mode demonstrates playback with up to 2 channels, up to 48 kHz sample rate and up to 16 bit width. This mode is enabled by default.
Multi-Channel - In this mode the device is enumerated as a UAC 5.1. This mode is disabled by default. See the Example configuration section to see how to enable the mode.
When playing an 5.1 audio file, the example sends only the front-left and front-right channels to the audio Line-Out port (the other channels are ignored), since this example only supports on-board codecs with stereo audio output.
As shown in the table below, the application is supported on several development boards, and each development board may have certain limitations, some development boards may also require hardware modifications or allow to use of an audio expansion board. Therefore, please check the supported features and Hardware modifications or Example configuration sections before running the demo.
| Mode | Standard | Multi-channel | ||
|---|---|---|---|---|
| Feature | Audio output [num of channels] | Audio output [num of channels] | ||
| On board codec | aud-exp-42448 | On board codec | aud-exp-42448 | |
| EVKC-MIMXRT1060 | 1-2 | X | 1-2 | X |
| EVKB-MIMXRT1170 | 1-2 | X | 1-2 | X |
| LPCXpresso55s69 | 1-2 | X | 1-2 | X |
| EVK-MCXN5XX | 1-2 | X | 1-2 | X |
| RW612BGA | X | X | X | X |
| RW612QFN | X | X | X | X |
Limitations:
Note:
If the USB device audio speaker example uses an ISO IN feedback endpoint, please attach the device to a host like PC which supports feedback function. Otherwise, there might be attachment issue or other problems.
Known issues:
No known issues.
More information about supported features can be found on the Supported features page.
Hardware requirements {#maestro-usb-speaker-HW-requirements}
Desired development board
2x Micro USB cable
Personal Computer
Headphones with 3.5 mm stereo jack
Hardware modifications {#maestro-usb-speaker-HW-modifications}
Some development boards need some hardware modifications to run the application. If the development board is not listed here, its default setting is required.
Preparation {#maestro-usb-speaker-preparation}
Connect the first micro USB cable between the PC host and the debug USB port on the development board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Connect the second micro USB cable between the PC host and the USB port on the development board.
Insert the headphones into Line-Out connector (headphone jack) on the development board.
Either press the reset button on your development board or launch the debugger in your IDE to begin running the demo.
Running the demo {#maestro-usb-speaker-running-the-demo}
When the example runs successfully, you should see similar output on the serial terminal as below:
**********************************************
Maestro audio USB speaker solutions demo start
**********************************************
Copyright 2022 NXP
[APP_Shell_Task] start
>> usb_speaker -1
Starting maestro usb speaker application
The application will run until the board restarts
[STREAMER] Message Task started
Starting playing
[STREAMER] start usb speaker
Set Cur Volume : fbd5
Type help to see the command list. Similar description will be displayed on serial console:
>> help
"help": List all the registered commands
"exit": Exit program
"version": Display component versions
"usb_speaker": Play data from the USB port as an audio 2.0
speaker device.
USAGE: usb_speaker <seconds>
<seconds> Time in seconds how long the application should run.
When you enter a negative number the application will
run until the board restarts.
EXAMPLE: The application will run for 20 seconds: usb_speaker 20
Details of commands can be found here.
Example configuration {#maestro-usb-speaker-example-configuration}
The example can be configured by user. Before configuration, please check the table to see if the feature is supported on the development board.
Enable Multi-channel mode:
The feature can be enabled by set the
USB_AUDIO_CHANNEL5_1macro to1Uin theusb_device_descriptor.hfile.Note: When device functionality is changed, such as UAC 5.1, please uninstall the previous PC driver to make sure the device with changed functionality can run normally.
Functionality {#maestro-usb-speaker-functionality}
The Usb_speaker command calls the STREAMER_speaker_Create function from the app_streamer.cfile that creates pipeline with the following elements:
- ELEMENT_USB_SRC_INDEX
- ELEMENT_SPEAKER_INDEX
Playback itself can be started with the STREAMER_Start function.
Each of the elements has several properties that can be accessed using the streamer_get_property or streamer_set_property function. These properties allow a user to change the values of the appropriate elements. The list of properties can be found in streamer_element_properties.h. See the example of setting property value in the following piece of code from the app_streamer.c file:
ELEMENT_PROPERTY_T prop;
prop.prop = PROP_USB_SRC_SET_SAMPLE_RATE;
prop.val = AUDIO_SAMPLING_RATE;
streamer_set_property(handle->streamer, 0, prop, true);
prop.prop = PROP_USB_SRC_SET_NUM_CHANNELS;
prop.val = 2;
streamer_set_property(handle->streamer, 0, prop, true);
prop.prop = PROP_USB_SRC_SET_FRAME_MS;
prop.val = 1;
streamer_set_property(handle->streamer, 0, prop, true);
Some of the predefined values can be found in the streamer_api.h.
States {#maestro-usb-speaker-states}
The application can be in 2 different states:
Idle
Running
Commands in detail {#maestro-usb-speaker-commands-in-detail}
Legend for diagrams: @mermaid{legend}
help, version {#maestro-usb-speaker-help-version}
@mermaid{help_version2}
usb_speaker <seconds> {#maestro-usb-speaker-usb-speaker}
@mermaid{maestro-usb-speaker-usb-speaker}