Maestro record example
Table of content
Overview {#maestro-record-overview}
The Maestro record example demonstrates audio processing on the ARM cortex core utilizing the Maestro Audio Framework library.
The application is controlled by commands from a shell interface using serial console.
Depending on target platform or development board there are different modes and features of the demo supported.
Loopback - The application demonstrates a loopback from the microphone to the speaker without any audio processing. Mono, stereo or multichannel mode can be used, depending on the hardware, see table below.
File recording - The application takes audio samples from the microphone inputs and stores them to an SD card as an PCM file. The PCM file has following parameters:
Mono and stereo : 2 channels, 16kHz, 16bit width
Multi-channel (AUD-EXP-42448): 6 channels, 16kHz, 32bit width
Voice control - The application takes audio samples from the microphone input and uses the VIT library to recognize wake words and voice commands. If a wake word or a voice command is recognized, the application write it to the serial terminal.
Encoding - The application takes PCM samples from memory and sends them to the Opus encoder. The encoded data is stored in memory and compared to a reference. The result of the comparison is finally written into the serial terminal.
As shown in the table below, the application is supported on several development boards, and each development board may have certain limitations, some development boards may also require hardware modifications or allow to use of an audio expansion board. Therefore, please check the supported features and Hardware modifications or Example configuration sections before running the demo.
| Mode | Loopback | File recording | Voice control | Encoding | ||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Feature | Audio input / output [num of channels] | Audio inputs [num of channels] | Audio inputs [num of channels] | Additional libraries | Encoder | |||||||
| On board codec | DMICs | aud-exp-42448 | On board codec | DMICs | aud-exp-42448 | On board codec | DMICs | aud-exp-42448 | VIT | VoiceSeeker | OPUS | |
| EVKC-MIMXRT1060 | 1 / 1 | X | 1-6 / 1-6 | 1 | X | 1-6 | 1 | X | 1-2 | OK | OK | OK |
| EVKB-MIMXRT1170 | 0 / 1-2 | 1-2 | X | X | 1-2 | X | X | 1-2 | X | OK | OK | OK |
| LPCXpresso55s69 | 1-2 / 1-2 | X | X | 1-2 / 1-2 | X | X | 1 | X | X | OK | X | X |
| EVK-MCXN5XX | 1-2 / 1-2 | X | X | 1-2 | X | X | 1-2 | X | X | OK | X | OK |
| RW612BGA | 0 / 1-2 | 1-2 | X | X | X | X | X | 1-2 | X | OK | OK | X |
| RW612QFN | 0 / 1-2 | 1-2 | X | X | X | X | X | 1-2 | X | OK | OK | X |
Limitations:
Addition labraries
VIT:
The VIT is supported only in the MCUXpresso IDE and ARMGCC.
LPCXpresso55s69 - The VIT is disabled by default due to insufficient memory. To enable it, see the Example configuration section.
VoiceSeeker:
The VoiceSeeker is supported only in the MCUXpresso IDE and ARMGCC.
Encoder
OPUS:
LPCXpresso55s69 - The encoder is not supported due to insufficient memory.
The File recording mode is not supported on RW612BGA and RW612QFN development boards due to missing SD card slot.
Known issues:
EVKB-MIMXRT1170 - After several tens of runs (the number of runs is not deterministic), the development board restarts because a power-up sequence is detected on the RESET pin (due to a voltage drop).
More information about supported features can be found on the Supported features page.
Hardware requirements {#maestro-record-HW-requirements}
Desired development board
Micro USB cable
Headphones with 3.5 mm stereo jack
Personal computer
Optional:
SD card for file output
Audio expansion board AUD-EXP-42448 (REV B)
LPCXpresso55s69:
Source of sound with 3.5 mm stereo jack connector
Hardware modifications {#maestro-record-HW-modifications}
Some development boards need some hardware modifications to run the application. If the development board is not listed here, its default setting is required.
EVKB-MIMXRT1170:
Please remove below resistors if on board wifi chip is not DNP:
R228, R229, R232, R234
Please make sure R136 is weld for GPIO card detect.
EVK-MCXN5XX:
Short: JP7 2-3, JP8 2-3, JP10 2-3, JP11 2-3
RW612BGA and RW612QFN:
Connect: JP50; Disconnect JP9, JP11
Preparation {#maestro-record-preparation}
Connect a micro USB cable between the PC host and the debug USB port on the development board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Insert the headphones into the Line-Out connector (headphone jack) on the development board.
LPCXpresso55s69:
Insert source of sound to audio Line-In connector (headphone jack) on the development board.
Either press the reset button on your development board or launch the debugger in your IDE to begin running the demo.
Running the demo {#maestro-record-running-the-demo}
When the example runs successfully, you should see similar output on the serial terminal as below:
*******************************
Maestro audio record demo start
*******************************
Copyright 2022 NXP
[APP_SDCARD_Task] start
[APP_Shell_Task] start
>> [APP_SDCARD_Task] SD card drive mounted
Type help to see the command list. Similar description will be displayed on serial console:
>> help
"help": List all the registered commands
"exit": Exit program
"version": Display component versions
"record_mic": Record MIC audio and perform one (or more) of following actions:
- playback on codec
- perform VoiceSeeker processing
- perform voice recognition (VIT)
- store samples to a file.
USAGE: record_mic [audio|file|<file_name>|vit] 20 [<language>]
The number defines length of recording in seconds.
Please see the project defined symbols for the languages supported.
Then specify one of: en/cn/de/es/fr/it/ja/ko/tr as the language parameter.
For voice recognition say supported WakeWord and in 3s frame supported command.
Please note that this VIT demo is near-field and uses 1 on-board microphone.
NOTES: This command returns to shell after the recording is finished.
To store samples to a file, the "file" option can be used to create a file
with a predefined name, or any file name (without whitespaces) can be specified
instead of the "file" option.
"opus_encode": Initializes the streamer with the Opus memory-to-memory pipeline and
encodes a hardcoded buffer.
Details of commands can be found here.
Example configuration {#maestro-record-example-configuration}
The example can be configured by user. Before configuration, please check the table to see if the feature is supported on the development board.
Connect AUD-EXP-42448:
EVKC-MIMXRT1060:
Disconnect the power supply for safety reasons.
Insert AUD-EXP-42448 into J19 to be able to use the CS42448 codec for multichannel output.
Uninstall J99.
Set the
DEMO_CODEC_WM8962macro to0in theapp_definitions.hfileSet the
DEMO_CODEC_CS42448macro to1in theapp_definitions.hfile.Enable VoiceSeeker, see point bellow.
Note:
The audio stream is as follows:
Stereo INPUT 1 (J12) -> LINE 1&2 OUTPUT (J6)
Stereo INPUT 2 (J15) -> LINE 3&4 OUTPUT (J7)
Microphone (P1) & Microphone (P2) -> LINE 5&6 OUTPUT (J8)
Insert the headphones into the different line outputs to hear the inputs.
To use the Stereo INPUT 1, 2, connect an audio source LINE IN jack.
Enable VoiceSeeker:
On some development boards the VoiceSeeker is enabled by default, see the table above.
If more than one channel is used and VIT is enabled, the VoiceSeeker that combines multiple channels into one must be used, as VIT can only work with mono signal.
It is necessary to add
VOICE_SEEKER_PROCsymbol to preprocessor defines on project level:(Project -> Properties -> C/C++ Build -> Settings -> MCU C Compiler -> Preprocessor)
Enable VIT:
LPCXpresso55s69:
Remove
SD_ENABLEDandSTREAMER_ENABLE_FILE_SINKsymbols from preprocessor defines on project level.Add
VIT_PROCsymbol to preprocessor defines on project level:(Project -> Properties -> C/C++ Build -> Settings -> MCU C Compiler -> Preprocessor)
Change the
DEMO_MIC_CHANNEL_NUMsymbol value from2to1in theapp_definitions.hfile
VIT model generation:
For custom VIT model generation (defining own wake words and voice commands) please use https://vit.nxp.com/
Functionality {#maestro-record-functionality}
The record_mic or opus_encode command calls the STREAMER_mic_Create or STREAMER_opusmem2mem_Create function from the app_streamer.c file depending on the selected mode.
When the Loopback mode is selected, the command calls the
STREAMER_mic_Createfunction that creates a pipeline with the following elements:ELEMENT_MICROPHONE_INDEX
ELEMENT_SPEAKER_INDEX
When the File recording mode is selected, the command calls the
STREAMER_mic_Createfunction that creates a pipeline with the following elements: - ELEMENT_MICROPHONE_INDEX - ELEMENT_FILE_SINK_INDEXWhen the Voice control mode is selected, the command calls the
STREAMER_mic_Createfunction that creates a pipeline with the following elements: - ELEMENT_MICROPHONE_INDEX - ELEMENT_VOICESEEKER_INDEX (IfVOICE_SEEKER_PROCis defined) - ELEMENT_VIT_INDEXWhen the Encoding mode is selected, the command calls the
STREAMER_opusmem2mem_Createfunction that creates a pipeline with the following elements: - ELEMENT_MEM_SRC_INDEX - ELEMENT_ENCODER_INDEX - ELEMENT_MEM_SINK_INDEX
Recording itself can be started with the STREAMER_Start function.
Each of the elements has several properties that can be accessed using the streamer_get_property or streamer_set_property function. These properties allow a user to change the values of the appropriate elements. The list of properties can be found in streamer_element_properties.h. See the example of setting property value in the following piece of code from the app_streamer.c file:
ELEMENT_PROPERTY_T prop;
prop.prop = PROP_MICROPHONE_SET_NUM_CHANNELS;
prop.val = DEMO_MIC_CHANNEL_NUM;
streamer_set_property(handle->streamer, 0, prop, true);
prop.prop = PROP_MICROPHONE_SET_BITS_PER_SAMPLE;
prop.val = DEMO_AUDIO_BIT_WIDTH;
streamer_set_property(handle->streamer, 0, prop, true);
prop.prop = PROP_MICROPHONE_SET_FRAME_MS;
prop.val = DEMO_MIC_FRAME_SIZE;
streamer_set_property(handle->streamer, 0, prop, true);
prop.prop = PROP_MICROPHONE_SET_SAMPLE_RATE;
prop.val = DEMO_AUDIO_SAMPLE_RATE;
streamer_set_property(handle->streamer, 0, prop, true);
Some of the predefined values can be found in the streamer_api.h.
States {#maestro-record-states}
The application can be in 2 different states:
Idle
Running
Commands in detail {#maestro-record-commands-in-detail}
Legend for diagrams: @mermaid{legend}
help, version {#maestro-record-help-version}
@mermaid{help_version2}
record_mic audio <time> {#maestro-record-record-mic-audio}
@mermaid{maestro_record_record-mic-audio}
record_mic file <time> ; record_mic <file_name> <time> {#maestro-record-record-mic-file}
@mermaid{maestro_record_record-mic-file}
record_mic vit <time> <language> {#maestro-record-record-mic-vit}
@mermaid{maestro_record_record-mic-vit}
opus_encode {#maestro-record-opus_encode}
@mermaid{maestro_record_opus-encode}
Processing Time {#maestro-record-processing-time}
Typical execution times of the streamer pipeline for the EVKC-MIMXRT1060 development board are detailed in the following table. The duration spent on output buffers and reading from the microphone is excluded from traversal measurements. Three measured pipelines were considered. The first involves a loopback from microphone to speaker, supporting both mono and stereo configurations. The second pipeline is a mono voice control setup, comprising microphone and VIT blocks. The final pipeline is a stereo voice control setup, integrating microphone, voice seeker, and VIT blocks.
For further details of execution times on individual elements, please refer to the Processing Time document.
streamer |
|
|---|---|
microphone -> speaker 1 channel |
40 μs |
microphone -> speaker 2 channels |
115 μs |
microphone -> VIT |
7.4 ms |
microphone -> voice seeker -> VIT |
9.9 ms |