Evaluate an Example Project
Supported Boards
Use the west extension west list_project to understand the board support scope for a specified example
west list_project -p examples/demo_apps/hello_world [-t armgcc]
INFO: [ 1][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evk9mimx8ulp -Dcore_id=cm33]
INFO: [ 2][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbimxrt1050]
INFO: [ 3][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbmimxrt1060]
INFO: [ 4][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbmimxrt1170 -Dcore_id=cm4]
INFO: [ 5][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkbmimxrt1170 -Dcore_id=cm7]
INFO: [ 6][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkcmimxrt1060]
INFO: [ 7][west build -p always examples/demo_apps/hello_world --toolchain armgcc --config release -b evkmcimx7ulp]
...
Build the project
Use west build -h to see help information for west build command.
Compared to zephyr’s west build, MCUXpresso SDK’s west build command provides following additional options for mcux examples:
–toolchain: specify the toolchain for this build, default armgcc.
–config: value for CMAKE_BUILD_TYPE, default debug.
–show-configs: show all supported build configurations for the project.
Here are some typical usage for generating a SDK example:
# Generate example with default settings
west build -b frdmk22f examples/demo_apps/hello_world
# Just print cmake commands, do not execute it
west build -b frdmk22f examples/demo_apps/hello_world --dry-run
# Generate other toolchain like iar, default armgcc
west build -b frdmk22f examples/demo_apps/hello_world --toolchain iar
# Generate config type, default debug
west build -b frdmk22f examples/demo_apps/hello_world --config release
# Show all supported build configurations
west build -b frdmk22f examples/demo_apps/hello_world --show-configs
For multicore devices, you shall specify the corresponding core id by passing the command line argument “-Dcore_id”. For example
west build -b evkmimxrt1170 examples/demo_apps/hello_world --toolchain iar -Dcore_id=cm7 --config flexspi_nor_debug
For shield, please use the “–shield” to specify the shield to run, like
west build -b mimxrt700evk --shield a8974 examples examples/issdk_examples/sensors/fxls8974cf/fxls8974cf_poll -Dcore_id=cm33_core0
Sysbuild(System build)
To support multicore project building, we ported Sysbuild from Zephyr. It supports combining multiple projects for compilation. You can build all projects by adding “–sysbuild” for main application. For example:
west build -b evkmimxrt1170 --sysbuild ./examples/middleware/multicore/multicore_examples/hello_world/primary -Dcore_id=cm7 --config flexspi_nor_debug -p always
Config a project
Example in MCUXpresso SDK is configured and tested with pre-defined configuraiton. You can follow this step to change the configuration.
Run cmake configuration
west build -b frdmk22f examples/demo_apps/hello_world --cmake-only
You can ignore --cmake-only, then the project will be built.
Run guiconfig target
west build -t guiconfig
Then you will get the Kconfig GUI launched, like

You can select/deselect and modify to do reconfiguration and remember to save.
After you save and close, you can directly run “west build” to do the build.
Flash
Note: Please refer West Flash and Debug Support to enable west flash/debug support.
As we do not have a FRDM-K64F with JLink or other runners for test, we only ensure flash/debug commands can work for linkserver. Please install linkserver and add it to your PATH firstly.
Flash the hello_world example:
west flash -r linkserver
Debug
Start a gdb interface by following command:
west debug -r linkserver