This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dspi_interrupt

Overview

The dspi_interrupt example shows how to use DSPI driver in interrupt way:

In this example , one dspi instance used as DSPI master and another dspi instance used as DSPI slave in the same board. This example does not use the transactional API in DSPI driver. It’s a demonstration that how to use the interrupt in KSDK driver.

  1. DSPI master send/received data to/from DSPI slave in interrupt . (DSPI Slave using interrupt to receive/send the data)

Supported Boards