This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Hardware requirements

  • Micro USB cable

  • rdrw610 board

  • Personal Computer

Board settings

U38 DIP 1,2,3,4 all off HD12 1-2, 3-4 connected

Prepare BLE controller

Download BLE controller FW according to the document component\conn_fwloader\readme.txt.

Note: To ensure that the LITTLEFS flash region has been cleaned, all flash sectors need to be erased before downloading example code. After downloaded binary to the target board, please reset the board by pressing SW5 or power off and on the board to run the application.