Hardware requirements
FRDM-MCXA156 board
USB-C cable
Personal Computer
Board settings
MCUBoot layout is the following:
MCUBoot region 0x0 - 0x08000 : 32kB Primary slot 0x8000 - 0x84000 : 496kB (0x7c000 bytes) Secondary slot 0x84000 - 0x100000 : 496kB (0x7c000 bytes)
MCUBoot header size is set to 512 bytes
Signing algorithm is ECDSA-P256
Write alignment is 16 bytes
Uses image swapping by
SWAP_USING_MOVE
Image signing example:
imgtool sign –key sign-ecdsa-p256-priv.pem –align 16 –version 1.1 –slot-size 0x7c000 –header-size 0x200 –pad-header –max-sectors 64 ota_mcuboot_basic.bin ota_mcuboot_basic.SIGNED.bin
If you experience problems with flash erase, check correct configuration
of ACL_SEC_x fields in CMPA region.