This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Build an example application {#GUID-151EFC23-F84E-4EB4-8940-5A8E58C7E348}

Do the following steps to build the hello_world example application.

  1. Open the desired demo application workspace. Most example application workspace files can be located using the following path:

    <install_dir>/boards/<board_name>/<example_type>/<application_name>/iar
    

    Using the LPCXpresso55S69 hardware platform as an example, the hello_world workspace is located in:

    <install_dir>/boards/lpcxpresso55s69/demo_apps/hello_world/iar/hello_world.eww
    

    Other example applications may have additional folders in their path.

  2. Select the desired build target from the drop-down menu.

    For this example, select hello_world – debug.

    |

|

  1. To build the demo application, click Make, highlighted in red in Figure 2.

    |

|

  1. The build completes without errors.

Parent topic:Run a demo application using IAR