Import Repository

The first operation in the proposed development flow in MCUXpresso for VS Code is to import a software repository. A software repository may have different sources supported by this extension: MCUXpresso SDK or Zephyr.

In order to achieve this, go to the MCUXpresso for VS Code extension, Imported Repositories option and press the ‘+’ symbol in the upper right of the toolbar (Help text will display ‘Import Local/Remote Repository’ when hovering over symbol. Alternatively use link found in Quickstart Panel)

Note: The big blue “Import repository” button is only available until the first repository is imported to the workspace.

Import SDK

Note: Regardless of the repository type (“Remote”, “Remote Archive”, or “Local Archive”), the installation path for the repository is highlighted inside the wizard page. This allows you to verify the destination before confirming the operation.


MCUXpresso SDK

For MCUXpresso SDK repository installation, please follow MCUXpresso SDK related documentation on MCUXpresso SDK

Zephyr

For Zephyr repository installation, please follow Zephyr related documentation on Zephyr

Other repository operations

Import local Git repository

If a user already has a software repository in a local directory, they can directly import the folder by using the “LOCAL” option.

Install local GIT

Remove or delete a repository

Each repository can be removed from the visible area without deleting it from disk:

Remove repository

A confirmation dialog will appear before removing the repository from the visible area:

Remove repository

The confirmation dialog is always shown when:

  • The repository has workspace projects associated with it (a list of affected projects is displayed in the dialog).

Remove Associated repository

  • The repository is being permanently deleted from disk.

Delete repository

When none of the above conditions apply, the confirmation dialog is shown by default. It can be suppressed by:

Note: The Yes, don’t ask again option is not available when the repository has associated projects or when permanently deleting from disk, as confirmation is always required in those cases.

Repositories can be permanently deleted from disk by selecting the delete option from the context menu:

Remove repository

Refresh repositories

If changes were made to one or more repositories, the “Refresh repositories” button from the toolbar can be used to update the information displayed in the view.

Refresh repository

Note: The button also invalidates the cached data so a subsequent load will be slower.

Update repository

An existing repository may also be updated via the west update command.

Update repository

Source Control extension

Once a repository is imported, the Source Control view within Visual Studio Code will track all sub-repositories that constitute the given git repository. This is a useful utility for monitoring changes made during development.

Source control repository

Terminal

Context menu for an imported repository provides access to the integrated terminal, allowing direct command execution within the repository directory.

Terminal repository